Latest shipping version:
Recent Firmware History:
Version: 1.4.128.116
Details:
Release: 9/8/2015
Bugs Fixed:
1.) When making a RUN to STOP mode transition with the Productivity3000 CPU mode switch, the “Stop Program� instruction in ladder or from the connected programming software, and there is an active output on the P3-HSO; it is possible that the output may pause and then continue the output pulses for a short period of time..
Note: Version 1.4.128.115 never shipped on production units, it was only available for download.
Version: 1.4.128.63
Details:
February 26, 2014
Bugs fixed:
1. Channel Velocity Feedback Tags may glitch positive while moving negative or at the start of HOME move when home position not set at zero.
Version: 1.4.128.60
Details:
May 8, 2013
Bugs fixed:
1. Enabling a HOME instruction set to mode 4 (Move to Switch 1 and Return), if on the return Switch 1 is missed, the physical limit switch for that direction is ignored.
Version: 1.4.128.58
Details:
April 30, 2013
Bugs Fixed:
1. Find Home (HOME) instruction fail when a general purpose input that is not designated as the Home sensor input is activated when the HOME instruction is triggered.
2. Velocity Move (VMOV) instructions fail under certain circumstances after aborting a 'Find Home' instruction. Can only be recovered after a Power On Reset.
Version: 1.4.128.49
Details:
April 25, 2012
Initial Launch Firmware