Latest shipping version:
Recent Firmware History:
Version: 1.1.15.109
Details:
Hardware:
1) Support for new USB chip on P3 backplanes.
Version: 1.1.15.97
Details:
Version: 1.1.14.38
Details:
FW 1.1.14.38 Release Notes
December 4, 2013
Bugs fixed:
1) P3-Remote expansion base output module(s) have "flashing" data after unplug then replug of the USB cable.
Notes:
1) This version of firmware is supported with 1.9.0.13 and higher of the Productivity Suite software.
2) Revision D1 & higher of the P3-550 downgrading firmware to older than 1.1.14.38 will cause LCD to display incorrectly. Please contact tech support for additional support @ 1(800)633-0405.
3) Revision D & lower of the P3-550 upgrading to 1.1.14.38 firmware will cause LCD display issue. Please power cycle P3-550 to fix this issue.
Version: 1.1.13.17
Details:
FW 1.1.13.17 Release Notes
December 6, 2012
Improvements:
1. New Remote Slave MST bit 'Module Ready' that indicates good communication to the P3-550.
Bugs fixed:
1. CPI instruction running on RS serial port does not verify CRC.
Version: 1.1.12.14
Details:
FW Release Notes 1.1.12.14
April 25, 2012
*Note: All P3-RS versions 1.1.11.28 or older were combined with the P3-550 firmware file. Please refer to the P3-550 firmware file for any P3-RS improvements & bug fixes.
Improvements:
1. Support for new P3-HSO, P3-HSI & P2-16TD3P now supported.
2. Support for new P3 firmware packages (.adfw)
Bugs fixed:
1. MRX and MWX do not work correctly with more than 255 tags.
2. Clock set tags extended Modbus address are broken.