Latest shipping version:
Recent Firmware History:
Version: 5.3.192
Details:
Major New Features
• Security enhancements
Bug Fixes
• Fixed problem where some switches did not correctly apply settings when an SFP is installed resulting in fiber issues.
• Fixed incorrect initialization of 16MS and 18MG switches which could result in two switches calculating identical port MAC addresses.
• Fixed inability to configure DHCP server when upgrading from pre-5.3 series firmware to 5.3 series firmware.
• Fixed DHCP server was passing the switch as the gateway when the switch has a gateway configured itself. Now, if the switch has a configured gateway, that will be passed as the gateway to DHCP clients. If it does not, the switch's IP will be sent as the gateway address.
• Removed validation which would incorrectly flag some non-broadcast IPv4 addresses as broadcast, which would, in turn, not allow you to set the IPv4 address to a valid address.
• Fixed possible missed state transitions if there is more than one Spanning Tree Instance.
Version: 5.3.174
Details:
new features and bug fixes are listed in the readme file. This version includes security improvements for switch management interface access
Version: 5.0.190
Details:
Initial version
Supports:
SE-SW5M, SE-SW5M-2SC, SE-SW5M-2ST,
SE-SW8M, SE-SW8M-2SC, SE-SW8M-2ST,
SE-SW8MG-4P, SE-SW10MG-2P
SE-SW16M