Latest shipping version:
Recent Firmware History:
Version: P2-All_In_One_20240513
Details:
P2000 Firmware History
Latest firmware file: P2-All_In_One_20240513.adfw
P2-All_In_One_20240513 contains the following individual firmware versions:
P2-622 version 1.7.2.11 (new)
P2-550 version 1.3.0.6 (new)
P2-RS version 1.2.9.21
P2-SCM version 1.1.128.87
P2-HSI version 1.3.128.9
P2-HSO version 1.4.128.116
P2-04B version 1.0.16.0
P2-07B version 1.0.16.0
P2-11B version 1.0.16.0
P2-15B version 1.0.16.0
==========================================
P2-622 Firmware
Latest shipping version: Version: 1.7.2.11
Firmware Version History:
P2-622 Version: 1.7.2.11 Release Date: May 22, 2024
Note: P2-622: The steps below are required prior to downloading a project in version 4.2 or higher to prevent the CPU from showing a 'spinner' on the LCD and requiring a power cycle.
1. First, use any version of Productivity Suite to upgrade the P2-622 firmware to version 1.7.2.11.
2. Then, transfer a Productivity Suite v4.2.0.x or higher project to the P2-622 CPU.
Bugs Fixed:
1.) CSI-Read (Ascii) changing Max Number of Bytes to 1 while sending 128 bytes from another CPU causes USB connection to drop and will not recover until power cycle.
===========================================
P2-550 Firmware
Latest shipping version: Version: 1.3.0.6
Firmware Version History:
P2-550 Version: 1.3.0.6 Release Date: May 22, 2024
Improvements:
1.) Security Updates
Version: P2-All_In_One_20231106
Details:
Improvements:
1.) Add support for new communications instructions for P2-622 CPU
P2000 Firmware History
Latest firmware file: P2-All_In_One_20231106.adfw
P2-All_In_One_20231106 contains the following individual firmware versions:
P2-622 version 1.7.2.8 (new)
P2-550 version 1.2.10.10
P2-RS version 1.2.9.21
P2-SCM version 1.1.128.87
P2-HSI version 1.3.128.9
P2-HSO version 1.4.128.116
P2-04B version 1.0.16.0
P2-07B version 1.0.16.0
P2-11B version 1.0.16.0
P2-15B version 1.0.16.0
====================
P2-622 Firmware
Latest shipping version: Version: 1.7.2.8
Firmware Version History:
Version: 1.7.2.8 Release Date: November 29th, 2023
Bugs Fixed:
1.) Micro SD card LED can remain on even when no card is mounted
2.) Micro SD card does not always install and mount
3.) DNS Server address field and Default Gateway field do not always accept new address until power cycle
4.) Serial comms may fail until CPU run mode is toggled, if P2-SCM and P2-HSI/HSO are in the system and in use
5.) USB IP address can become unusable in some cases
6.) P2-622 can experience watchdog with extremely heavy external ethernet traffic
7.) P2-622 can experience serial communications traffic failure due to packet validation issues
Version: P2-All_In_One_20230425
Details:
P2000 Firmware History
Latest firmware file: P2-All_In_One_20230425.adfw
P2-All_In_One_20230425 contains the following individual firmware versions:
P2-622 version 1.7.1.11 (new)
P2-550 version 1.2.10.10
P2-RS version 1.2.9.21
P2-SCM version 1.1.128.87
P2-HSI version 1.3.128.9
P2-HSO version 1.4.128.116
P2-04B version 1.0.16.0
P2-07B version 1.0.16.0
P2-11B version 1.0.16.0
P2-15B version 1.0.16.0
====================
P2-622 Firmware
Latest shipping version: Version: 1.7.1.11
Firmware Version History:
Version: 1.7.1.11 Release Date: June 14, 2023
Initial release
Version: P2-All_In_One_20220718
Details:
P2000 Firmware History
Latest firmware file: P2-All_In_One_20220718.adfw
P2-All_In_One_20220718 contains the following individual firmware versions:
P2-550 version 1.2.10.10 (new)
P2-RS version 1.2.9.21 (new)
P2-SCM version 1.1.128.87
P2-HSI version 1.3.128.9
P2-HSO version 1.4.128.116
P2-04B version 1.0.16.0
P2-07B version 1.0.16.0
P2-11B version 1.0.16.0
P2-15B version 1.0.16.0
====================
P2-550 Firmware
Latest shipping version: Version: 1.2.10.10
Firmware Version History:
*******
Version: 1.2.10.10 Release Date: July 25, 2022
New feature:
1.) Changed to allow Modbus access to a single Modbus address within an S32/F32 tag
2.) Implemented fix for Large Block NAND sector fault
====================
P2-RS Firmware
Latest shipping version: Version: 1.2.9.21
Firmware Version History:
*******
Version: 1.2.9.21 Release Date: July 25, 2022
Hardware:
1.) Implemented fix for Large Block NAND sector fault
++++++++++
Version: P2-All_In_One_20211026
Details:
P2000 Firmware History
Latest firmware file: P2-All_In_One_20211026.adfw
P2-All_In_One_20211026 contains the following individual firmware versions:
P2-550 version 1.2.10.6 (new)
P2-RS version 1.2.9.20
P2-SCM version 1.1.128.87
P2-HSI version 1.3.128.9
P2-HSO version 1.4.128.116
P2-04B version 1.0.16.0
P2-07B version 1.0.16.0
P2-11B version 1.0.16.0
P2-15B version 1.0.16.0
====================================================================================================
P2 All-In-One Firmware
Latest shipping version: Version: P2-All_In_One_20211026
Firmware Version History:
*******
Version: P2-All_In_One_20211026 Release date: March 30, 2022
Contains:
P2-550 version 1.2.10.6 (new)
P2-RS version 1.2.9.20
P2-SCM version 1.1.128.87
P2-HSI version 1.3.128.9
P2-HSO version 1.4.128.116
P2-04B version 1.0.16.0
P2-07B version 1.0.16.0
P2-11B version 1.0.16.0
P2-15B version 1.0.16.0
*******
Version: P2-All_In_One_20210812 Release date: September 14, 2021
Contains:
P2-550 version 1.2.9.41 (new)
P2-RS version 1.2.9.20 (new)
P2-SCM version 1.1.128.87
P2-HSI version 1.3.128.9
P2-HSO version 1.4.128.116
P2-04B version 1.0.16.0
P2-07B version 1.0.16.0
P2-11B version 1.0.16.0
P2-15B version 1.0.16.0
*******
Version: P2-All_In_One_20210629 Release date: July 29, 2021
Contains:
P2-550 version 1.2.9.38 (new)
P2-RS version 1.2.9.17 (new)
P2-SCM version 1.1.128.87
P2-HSI version 1.3.128.9
P2-HSO version 1.4.128.116
P2-04B version 1.0.16.0
P2-07B version 1.0.16.0
P2-11B version 1.0.16.0
P2-15B version 1.0.16.0
====================================================================================================
P2-550 Firmware
Latest shipping version: Version: 1.2.10.6
Firmware Version History:
*******
Version: 1.2.10.6 Release Date: March 30, 2022
New feature:
1.) Added DNS support for new MQTT feature in Productivity Suite 3.11.0.x.
*******
Version: 1.2.9.41 Release date: September 14, 2021
Hardware:
1.) This release includes an update to firmware due to updated OLED screen (UIM) hardware.
Note: P2-550 firmware may be downgraded once. However, once downgraded, if the firmware is downgraded a second time, the UIM will become completely blank. UIM functionality can be restored by upgrading to the latest firmware version.
*******
Version: 1.2.9.38 Release date: July 29, 2021
Bug Fixes:
1.) P2-CPU Goes to RUN immediately after E01005 occurring instead of forcing to STOP
2.) P2-550 with duplicate remote slave IDs does not display duplicate base ID error
*******
Version: 1.2.9.33 Release date: May 3, 2021
Bugs fixed:
1.) Cannot Save project to uSD card from OLED menu.
2.) Firmware update corrupting CPU if bad sector found.
*******
Version: 1.2.9.30 Release date: February 18, 2021
Bugs fixed:
1.) Web Server access to Data Log file only showing data from first access due to caching. This fix applies to Chrome and Edge only.
2.) Load project from uSD card will fail if CPU has no existing project
3.) CPU hardware revision E, cannot load project from uSD card
*******
Version: 1.2.9.28 Release date: September 21, 2020
Bugs fixed:
1.) Incomplete data flush to PMD (portable memory device) upon PMD Eject
2.) Incomplete data flush to PMD upon EPF (early power fail) event
3.) Modbus TCP Server. When writing a block of mixed 32-bit and 16-bit integers
to the PLC, the data can get written to the wrong location and return an illegal
data address exception in certain situations
4.) Abnormal IGMP traffic causes Watchdog
*******
Version: 1.2.9.17 Release Date: June 19, 2020
Note: This firmware requires Productivity Suite Version 3.5.x or higher
Improvements:
1.) Added support for P2-550 CPU Hardware Rev. E (Large Block NAND)
2.) Added support for P2-02HSC, P2-04PWM, P2-01DC, P2-04AD-1, P2-04AD-2, P2-04DA-1, P2-04DA-2 modules
Bugs fixed:
1.) Modbus RTU lockup when noise received during transmit
2.) Cannot upgrade firmware over Ethernet during Service Mode
3.) Mulitple Email (EMAL) instructions (20+) may cause CPU to crash immediately on Run Mode transition
4.) Ethernet Heartbeat Timeout bit (MST-0.0.0.65) not working
5.) Problem loading Project from SD Card
*******
Version: 1.2.9.9 Release Date: October 30, 2019
Improvements:
1.) Added 2 new error codes E04206 (MemDev near file cnt limit) and E04207 (MemDev file cnt limit)
2.) Eject memory device when 200 file limit reached
Bugs fixed:
1.) P2-CPU may crash for E01005 during system power up with certain module set up
2.) FPGA improvement
*******
Version: 1.2.7.39 Release Date: June 10, 2019
Bugs fixed:
1.) CPU may lockup with serial Modbus instructions when transitioning Run-Stop.
*******
Version: 1.2.7.37 Release date: December 12, 2018
Improvements:
1.) Added support for new features:
a. Secure integrated Email
b. Network Time Service
c. Domain Name Server
Bugs fixed:
1.) Modbus RTU, as slave, does not show exception for unknown Function Codes.
2.) CPU date not changing correctly if set to some older time frames.
3.) Heavy Modbus master & slave communication may cause Watchdog timeout.
4.) Modbus RTU/TCP with MRX/MWX operation gets stuck "InProgress" after a Runtime Project Transfer.
5.) First containing ModBus/TCP non-existing devices in call task takes 2x longer than subsequent scans.
6.) CPU flash memory may become corrupted during project transfer.
7.) GUI can not discover any IO modules from P2-RS USB access point.
8.) Only the first 4 CPoE devices work. Not able to Send or Receive on the 5th (or higher) connection.
9.) CPU Ethernet port ready bit does not ever show true under/after certain conditions.
10.) CPU may go into reboot mode if project contains multiple Modbus MWX or MRX instructions to same device.
11.) Cannot change the CPU Gateway address from the CPU Property Panel.
12.) On project transfer via USB error "Could not transfer the project from the CPU".
*******
Version: 1.2.2.77 Release date: August 1, 2018
Bugs fixed:
1.) CPU is not handling MWX/MRX instruction timeouts correctly.
*******
Version: 1.2.2.76 Release Date: January 24, 2018
Bugs fixed:
1.) Mitigate effects on CPU when the external Ethernet port on the CPU experiences irregular Ethernet traffic.
*******
Version: 1.2.2.75 Release Date: November 28, 2017
Bugs fixed:
1.) System discovery and project transfer fails resulting in E01201 Sema Obtain error. This may happen when on a network with other devices using broadcast messages.
2.) Repeated consecutive power cycles may force CPU to stop mode and corrupt NAND flash.
3.) When there were multiple pending Modbus TCP Requests over the same TCP connection the PLC would send incomplete Responses and close the TCP connection.
It is now changed so that the first three Requests will receive Responses. The remaining Requests will receive Exception Response 6: Slave Busy.
Note: This version of firmware requires version 2.2.X or higher of the Productivity Suite software.
*******
Version: 1.2.2.69 Release Date: July 6, 2017
Bugs fixed:
1.) Incurring drop packets during project transfer via Ethernet may cause the transfer to fail.
2.) Updated initialization sequence for discrete outputs.
Note: This version of firmware requires version 2.2.X or higher of the Productivity Suite software.
*******
Version: 1.2.2.64 Release Date: August 9, 2016
Bugs fixed:
1.) P2-CPU fails discover any GS Drives after initial project download.
Note: This version of firmware requires version 2.2.X or higher of the Productivity Suite software.
*******
Version: 1.2.2.59 Release Date: April 6, 2016
Bugs fixed:
1.) P2-CPU, as an EIP scanner, may reset with explicit IO message in multicast mode setting.
2.) P2-CPU with P2-SCM CPO_CPI project becomes unresponsive and causes an E01005 error.
Improvements:
1.) Support for new modules P2-08NTC & P2-RS
Note: This version of firmware is supported with 2.2.0.12 and higher of the Productivity Suite software.
*******
Version: 1.2.1.21 Release Date: March 2, 2016
Bugs fixed:
1.) P2-550 remains in run mode when CPU loses communication with the local base.
*******
Version: 1.2.1.15 Release Date: June 22, 2015
Bugs fixed:
1.) P2-550 with MODBUS TCP and RTU(485) Client and server may have E01005 error occur under heavy packet lost/retransmission
*******
Version: 1.2.1.13 Release Date: April 22, 2015
Initial release
====================================================================================================
P2-Base Firmware
Latest shipping version: Version: 1.0.16.0
Firmware Version History:
*******
Version: 1.0.16.0 Release Date: August 9, 2016
Improvements:
1.) Improved how the base handles loss of communication with CPU.
Note: This version of firmware requires version 2.2.X or higher of the Productivity Suite software.
*******
Version: 1.0.15.0 Release Date: June 22, 2015
Bugs fixed:
1.) If P2-550 is removed while system power is on. Outputs that were on when P2-550 was removed will remain on until base is power cycled.
*******
Version: 1.0.14.0 Release Date: April 22, 2015
Initial release
====================================================================================================
P2-HSI Firmware
Latest shipping version: Version: 1.3.128.9
Firmware Version History:
*******
Version: 1.3.128.9 Release Date: October 3, 2019
Bugs fixed:
1.) We have discovered that in rare situations the P2-HSI module can become unresponsive
resulting in loss of status updates to other modules in the base leaving inputs and outputs in
their last known state.
*******
Version: 1.3.128.6 Release Date: June 10, 2019
Bugs fixed:
1.) Position Cannot Be Set Properly when Setting Channel to Rotary.
2.) General Purpose Output 1 Resets without Program Command After 130 sec.
3.) Current Velocity falls to zero during oscillation while traveling negative.
*******
Version: 1.3.128.5 Release Date: March 9, 2018
Bugs fixed:
1.) Px-HSI in Q1X Mode Reports Incorrect Negative Position in Linear Mode.
2.) Using Slow Mode in Velocity Estimator Could Produce Erratic Readings.
*******
Version: 1.3.128.4 Release Date: December 16, 2015
Improvements:
1.) Support for new Programmable Limit Switch (PLS) & Preset Table (PST) instructions.
*******
Version: 1.2.128.41 Release Date: April 22, 2015
Initial release
====================================================================================================
P2-HSO Firmware
Latest shipping version: Version: 1.4.128.116
Firmware Version History:
*******
Version: 1.4.128.116 Release date: March 26, 2021
Details:
Updated SROM data fields for production test. No change to module functionality.
*******
Version: 1.4.128.115 Release Date: August 6, 2015
Bugs fixed:
1.) If Velocity Move (VMOV) instruction is started at a commanded velocity of zero, then later commanded negatively, the Channel Velocity Feedback Tags reports positive for several scans.
2.) Fault Overload indication (either LED or Module Error Code) does not immediately occur on the fault condition.
3.) Find Home (HOME) instruction under certain conditions will cause an incorrect status move bit to be set.
*******
Version: 1.4.128.114 Release Date: April 22, 2015
Initial release
====================================================================================================
P2-RS Firmware
Latest shipping version: Version: 1.2.9.20
Firmware Version History:
*******
Version: 1.2.9.20 Release Date: September 14, 2021
Hardware:
1.) This release includes an update to firmware due to updated OLED screen (UIM) hardware.
Note: P2-RS firmware may be downgraded once. However, once downgraded, if the firmware is downgraded a second time, the UIM will become completely blank. UIM functionality can be restored by upgrading to the latest firmware version.
*******
Version: 1.2.2.69 Release Date: July 6, 2017
Bugs fixed:
1.) Updated initialization sequence for discrete outputs.
Note: This version requires GUI build 2.2.X or higher.
*******
Version: 1.2.2.64 Release Date: September 9, 2016
Bugs fixed:
1.) P2-RS will go into service mode when it loses communications to P2-CPU more than three times.
Note: This version requires GUI build 2.2.X or higher.
*******
Version: 1.2.2.58 Release Date: April 6, 2016
Initial release
====================================================================================================
P2-SCM Firmware
Latest shipping version: Version: 1.1.128.87
Firmware Version History:
*******
Version: 1.1.128.87 Release Date: August 9, 2016
Bugs Fixed:
1.) P2-SCM firmware update may fail, but shows success.
Note:This version requires GUI build 2.0.X or higher.
*******
Version: 1.1.128.81 Release Date: April 6, 2016
1.) Px-CPU with Px-SCM CPO_CPI project becomes unresponsive and causes an E01005 error
2.) Px-SCM RS485 as MODBUS slave device will require response time delay
3.) P2-SCM Comm stops; Requires CPU in STOP then SCM hotswap to restart comm
4.) SCM: Heartbeat Timeout Bit doesn't initialize on Stop to Run transition
5.) Px-SCM, ASCII Mode, Module Lockup while exploring Overflow conditions
*******
Version: 1.1.128.65 Release Date: April 22, 2015
Initial release