AutomationDirect Technical Support
AutomationDirect | Direct Sales in US and Canada | 1-800-633-0405

Productivity Series Frequently Asked Questions AutomationDirect Logo


Question

What is the speed of DC inputs for the PAC modules if I want to use them to count pulses? Can they be used like the High-Speed inputs on the 05/06?

Answer

The response time is given for each of the modules, and it's basically the same time as DirectLogic hardware.
However, the scan time of the P series CPU is so much faster, that the inputs can be used into a counter, up to 200 times per sec (200 Hz). This is still not close to the 5 Khz range for the 05/06 inputs in HSI mode, but it is great improvement over standard DL inputs.


FAQ Subcategory: None

This item was last updated on 2016-11-11
Document ID: 1322


The information provided in the AutomationDirect knowledge base is provided "as is" without warranty of any kind. AutomationDirect disclaims all warranties, either express or implied, including the warranties of merchantability and fitness for a particular purpose. In no event shall AutomationDirect or its suppliers be liable for any damages whatsoever including direct, indirect, incidental, consequential, loss of business profits or special damages, even if AutomationDirect or its suppliers have been advised of the possibility of such damages. Some states do not allow the exclusion of limitation of liability for consequential or incidental damages so the foregoing limitation may not apply.


Copyright © 1999- AutomationDirect.com. ALL RIGHTS RESERVED