Product Selected: Productivity Series
Category Selected: CPU & Programming
Press "Ctrl-F" to search for specific words in this FAQ.
| Question: What is the maximum number of rungs that can be in a single task? |
| Answer: The maximum number of rungs allowed in any single task is 4096. This includes any subrungs. |
| FAQ ID: 1418 |
| Question: What is the default IP address of the Ethernet programming port the P3-530 and P3-550? |
| Answer: 10.10.10.10 |
| FAQ ID: 1464 |
| Question: Are there any restricted IP addresses or ranges not allowed with the Productivity Suite software? |
| Answer: Restricted IP addresses starting with: * 127 * 10.20 * 223.255.255.254 or higher |
| FAQ ID: 1577 |