AutomationDirect Technical Support
AutomationDirect | Direct Sales in US and Canada | 1-800-633-0405

FCC Part 15 Information AutomationDirect Logo


[Code of Federal Regulations]
[Title 47, Volume 1]
[Revised as of October 1, 2001]
From the U.S. Government Printing Office via GPO Access
[CITE: 47CFR15.103]

[Page 687-688]

TITLE 47--TELECOMMUNICATION

CHAPTER I--FEDERAL COMMUNICATIONS COMMISSION

PART 15--RADIO FREQUENCY DEVICES--Table of Contents

Subpart B--Unintentional Radiators

Sec. 15.103 Exempted devices.

The following devices are subject only to the general conditions of operation in Secs. 15.5 and 15.29 and are exempt from the specific technical standards and other requirements contained in this part. The operator of the exempted device shall be required to stop operating the device upon a finding by the Commission or its representative that the device is causing harmful interference. Operation shall not resume until the condition causing the harmful interference has been corrected. Although not mandatory, it is strongly recommended that the manufacturer of an exempted device endeavor to have the device meet the specific technical standards in this part.

  • (a) A digital device utilized exclusively in any transportation vehicle including motor vehicles and aircraft.
  • (b) A digital device used exclusively as an electronic control or power system utilized by a public utility or in an industrial plant. The term public utility includes equipment only to the extent that it is in a dedicated building or large room owned or leased by the utility and does not extend to equipment installed in a subscriber's facility.
  • (c) A digital device used exclusively as industrial, commercial, or medical test equipment.
  • (d) A digital device utilized exclusively in an appliance, e.g., microwave oven, dishwasher, clothes dryer, air conditioner (central or window), etc.
  • (e) Specialized medical digital devices (generally used at the direction of or under the supervision of a licensed health care practitioner) whether used in a patient's home or a health care facility. Non-specialized medical devices, i.e., devices marketed through retail channels for use by the general public, are not exempted. This exemption also does not apply to digital devices used for record keeping or any purpose not directly connected with medical treatment.
  • (f) Digital devices that have a power consumption not exceeding 6 nW.
  • (g) Joystick controllers or similar devices, such as a mouse, used with digital devices but which contain only non-digital circuitry or a simple circuit to convert the signal to the format required (e.g., an integrated circuit for analog to digital conversion) are viewed as passive add-on devices, not themselves directly subject to the technical standards or the equipment authorization requirements.
  • (h) Digital devices in which both the highest frequency generated and the highest frequency used are less than 1.705 MHz and which do not operate from the AC power lines or contain provisions for operation while connected to the AC power lines. Digital devices that include, or make provision for the use of, battery eliminators, AC adaptors or battery chargers which permit operation while charging or that connect to the AC power lines indirectly, obtaining their power through another device which is connected to the AC power lines, do not fall under this exemption.
  • (i) Responsible parties should note that equipment containing more than one device is not exempt from the technical standards in this part unless all of the devices in the equipment meet the criteria for exemption. If only one of the included devices qualifies for exemption, the remainder of the equipment must comply with any applicable regulations. If a device performs more than one function and all of those functions do not meet the criteria for exemption, the device does not qualify for inclusion under the exemptions.

 

[Code of Federal Regulations]
[Title 47, Volume 1]
[Revised as of October 1, 2001]
From the U.S. Government Printing Office via GPO Access
[CITE: 47CFR15.5]

[Page 671]

TITLE 47--TELECOMMUNICATION

CHAPTER I--FEDERAL COMMUNICATIONS COMMISSION

PART 15--RADIO FREQUENCY DEVICES--Table of Contents

Subpart A--General

Sec. 15.5 General conditions of operation.

  • (a) Persons operating intentional or unintentional radiators shall not be deemed to have any vested or recognizable right to continued use of any given frequency by virtue of prior registration or certification of equipment, or, for power line carrier systems, on the basis of prior notification of use pursuant to Sec. 90.63(g) of this chapter.
  • (b) Operation of an intentional, unintentional, or incidental radiator is subject to the conditions that no harmful interference is caused and that interference must be accepted that may be caused by the operation of an authorized radio station, by another intentional or unintentional radiator, by industrial, scientific and medical (ISM) equipment, or by an incidental radiator.
  • (c) The operator of a radio frequency device shall be required to cease operating the device upon notification by a Commission representative that the device is causing harmful interference. Operation shall not resume until the condition causing the harmful interference has been corrected.
  • (d) Intentional radiators that produce Class B emissions (damped wave) are prohibited.

 

[Code of Federal Regulations]
[Title 47, Volume 1]
[Revised as of October 1, 2001]
From the U.S. Government Printing Office via GPO Access
[CITE: 47CFR15.29]

[Page 677]

TITLE 47--TELECOMMUNICATION

CHAPTER I--FEDERAL COMMUNICATIONS COMMISSION

PART 15--RADIO FREQUENCY DEVICES--Table of Contents

Subpart A--General

Sec. 15.29 Inspection by the Commission.

  • (a) Any equipment or device subject to the provisions of this part, together with any certificate, notice of registration or any technical data required to be kept on file by the operator, supplier or party responsible for compliance of the device shall be made available for inspection by a Commission representative upon reasonable request.
  • (b) The owner or operator of a radio frequency device subject to this part shall promptly furnish to the Commission or its representative such information as may be requested concerning the operation of the radio frequency device.
  • (c) The party responsible for the compliance of any device subject to this part shall promptly furnish to the Commission or its representatives such information as may be requested concerning the operation of the device, including a copy of any measurements made for obtaining an equipment authorization or demonstrating compliance with the regulations.
  • (d) The Commission, from time to time, may request the party responsible for compliance, including an importer, to submit to the FCC Laboratory in Columbia, Maryland, various equipment to determine that the equipment continues to comply with the applicable standards. Shipping costs to the Commission's Laboratory and return shall be borne by the responsible party. Testing by the Commission will be performed using the measurement procedure(s) that was in effect at the time the equipment was authorized or verified.

Copyright © 1999-2025 AutomationDirect.com. ALL RIGHTS RESERVED