AutomationDirect Technical Support
AutomationDirect | Direct Sales in US and Canada | 1-800-633-0405

CPU Communication Port Setup Parameters
DL260 Non Sequence (ASCII) AutomationDirect Logo



WORD 1
0000 0000 0000 aaaa
260: V7651
Data format
0000 = 7 data, 1 stop, none parity
0001 = 7 data, 2 stop, None parity
0010 = 7 data, 1 stop, Even parity
0011 = 7 data, 2 stop, Even parity
0100 = 8 data, 1 stop, None parity
0101 = 8 data, 2 stop, None parity
0110 = 8 data, 1 stop, Even parity
0111 = 8 data, 2 stop, Even parity
1010 = 7 data, 1 stop, Odd parity
1011 = 7 data, 2 stop, Odd parity
1110 = 8 data, 1 stop, Odd parity
1111 = 8 data, 2 stop, Odd parity

 

WORD 2
0000 0000 0aaa aaaa
260: V7652
Protocol Mode 
01110000 = No flow control 
01110001 = Xon/Xoff flow control 
01110010 = RTS flow control 
01110011 = Xon/Xoff and 
  RTS Flow control 

 

WORD 3 
260: V7654
V memory address for data
Hex value of the V location to temporary store the ASCII data coming in to the PLC. Set this to an unused V location

 

WORD 4
0yyy 0ttt mmmm mxxx

RTS On-delay
yyy
Communication Timeout
(in % of standard timeout)
ttt
Protocol Mode
mmmmm
RTS Off-delay
xxx
260: V7655
000 = 0mS
001 = 2mS
010 = 5mS
011 = 10mS
100 = 20mS
101 = 50mS
110 = 100mS
111 = 500mS
000 = 100%
001 = 120%
010 = 150%
011 = 200%
100 = 500%
101 = 1000%
110 = 2000%
111 = 5000%
00010 = Non Sequence
000 = 0mS
001 = 2mS
010 = 5mS
011 = 10mS
100 = 20mS
101 = 50mS
110 = 100mS
111 = 500mS

 

WORD 5
0000 e000 0000 0bbb

Echo Suppression
e
Baud Rate
bbb
260: V7656
0 = 232 or 422
1 = 485 2 wire
000 = 300  
001 = 600
010 = 1200
011 = 2400
100 = 4800
101 = 9600
110 = 19200
111 = 38400

 

WORD 6
260: V7657
The CPU will accept the setup values when a 'setup complete' flag is written to this V-memory location. For the 260 this flag is a value of K0500, representing the available port. When the CPU checks this value, it will change the '5' to an 'A' if the port settings have been accepted, or an 'E' if there was an error.

Copyright © 1999- AutomationDirect.com. ALL RIGHTS RESERVED