| |
STEP 1)
First, gather these required
materials:
- EZ-TOUCH PANEL (ANY SIZE)
- EZTOUCH-PGMCBL
- EZ-TOUCHEDIT
|
| |
STEP 2)
At this point, your EZ-TOUCHEDIT
software will need to be installed and your PC connected to the EZ-TOUCHPANEL
by the way of the EZTOUCH-PGMCBL. Now make sure the panel is powered up and the
software is open and running before proceeding.
|
 |
STEP 3)
This is the first screen
you should see when you start up the EZ-TOUCHEDIT software. When you get here,
click on the "Edit Program OFF-LINE" shown in the picture.
< Click on image for
larger picture
|
 |
STEP 4)
In this step you click
on "SETUP", then scroll down and click on "UPGRADE FIRMWARE...." See picture.
After you do this go to Step Five.
< Click on image for
larger picture
|
 |
STEP 5)
Now you click on the "BROWSE"
button. This will pop up another box that you will use to find where your firmware
is located. After you find the firmware file, you will click on it and then click
on "OPEN". Now proceed to Step Six.
< Click on image for
larger picture
|
 |
STEP 6)
In this step you will select
the PC Port you are using for you EZ-TOUCHPANEL. To do this you will click on
the drop box arrow in the "USE PC PORT" area. After selecting the COM Port click
"OK".
Then go to the next step.
< Click on image for
larger picture
|
 |
STEP 7)
If your PC finds the EZ-TOUCHPANEL
you should see this screen (shown in the picture). If you do not see this screen
an error has occurred . To correct this error, check your COM PORT connection,
cable connection and then go back to the beginning of this process. Now that you
are here you will click "CONTINUE". When you click continue then your firmware
update will start. Proceed on to the next step.
< Click on image for
larger picture
|
 |
STEP 8)
Once the Update tool reaches
100% completion, you will click on "OK". This is the end of the procedure. Go
to the next step to see how you test the EZ-TOUCHPANEL to see if the upgrade was
successful.
< Click on image for
larger picture
|
 |
STEP 9)
To test the firmware version
you will press with your finger tips the upper left corner of the screen and the
lower left corner of the screen simultaneously (shown below). When you do this,
a screen will come up with the version of your EZ-TOUCHPANEL to exit firmware
screen just powerdown.
Now you are now finished.
< Click on image for
larger picture
|