This is where you can get the AutoStart Utility, which allows you to configure Windows/NT so that you don't have to type in the logon password.
Think &
Do Studio 6.0 Terminator I/O Patch
In version 6.0 of Studio with Terminator EBC, if you pull out a module and replace
it with the incorrect module it will crash Studio. To correct this problem,
unzip this Eth60patch1.zip file and place the two files (Iodll32.dll and TnDether.dll)
into the Thinkndo/Bin directory. This problem will be Corrected in version 6.1.
Product Advisory for Think & Do Studio:
The utility to convert existing Think & Do Version 5.2 (or older) and Think
& Do Live projects to Studio will not be released until March 1, 2001. If you
have an urgent need related to an existing project, please contact Think & Do
at 1-800-722-6875.
For application notes, new drivers and other information go to the Entivity web site.