AutomationDirect logoScreenCreator Support Resources


ScreenCreator Downloads:

v1.17
Maintenance Release

Do not delete any existing ScreenCreator files!! This is a maintenance release, not a full install. You must have a previous version of ScreenCreator to install this upgrade.

Un-Zip the files to a temporary folder.

Double-click setup.exe and follow the directions.

DO NOT erase your currently installed ScreenCreator files. This is only a maintenance release and does not contain the full software package. Change the the default folder, if your current version of Screen Creator is located in a diferent location.

When launching V1.17 for the first time, select "Add to Library" in order to save any User-defined parts you may have created.

(File size = ~2.9MB)

train.exe This self-extracting executable contains a ScreenCreator project with very useful parts and screens. Unzip this file to the proper folder and, in ScreenCreator, Project>Restore... the Train.PRO file to restore the project.
trainab.exe This self-extracting executable contains a ScreenCreator project (for Allen-Bradley SLC 500 PLCs) with very useful parts and screens. Unzip this file to the proper folder and, in ScreenCreator, Project>Restore... the TrainAB.PRO file to restore the project.