Changes implemented in Release 4.0 of LookoutDirect and DLPlus

What's New in Version 4.0 (Build 25), 6 Sep 2004

Note: Build 25 contains updated device drivers only, there are no changes to the Lookout components. So, after installing this service pack, your copy of LookoutDirect will still appear as Build 19 (look in the About box). You can use the Version utility in DSLaunch to verify that the "DirectSOFT32 - Communications Server" components have been updated to 4.0.025.

What's New in Version 4.0 (Build 24), 25 May 2004

Note: Build 24 contains updated device drivers only, there are no changes to the Lookout components. So, after installing this service pack, your copy of LookoutDirect will still appear as Build 19 (look in the About box). You can use the Version utility in DSLaunch to verify that the "DirectSOFT32 - Communications Server" components have been updated to 4.0.024.

What's New in Version 4.0 (Build 23), 20 February 2004

Note: Build 23 contains updated device drivers only, there are no changes to the Lookout components. So, after installing this service pack, your copy of LookoutDirect will still appear as Build 19 (look in the About box). You can use the Version utility in DSLaunch to verify that the "DirectSOFT32 - Communications Server" components have been updated to 4.0.023.

What's New in Version 4.0 (Build 22), 10 September 2003

Note: Build 22 contains updated device drivers only, there are no changes to the Lookout components. So, after installing this service pack, your copy of LookoutDirect will still appear as Build 18 (look in the About box). You can use the Version utility in DSLaunch to verify that the "DirectSOFT32 - Communications Server" components have been updated to 4.0.022.

What's New in Version 4.0 (Build 20), 27 June 2003

Note: Build 20 contains updated device drivers only, there are no changes to the Lookout components. So, after installing this service pack, your copy of LookoutDirect will still appear as Build 18 (look in the About box). You can use the Version utility in DSLaunch to verify that the "DirectSOFT32 - Communications Server" components have been updated to 4.0.020.

What's New in Version 4.0 (Build 18), 9 December 2002

What's New in Version 4.0 RC 1, 24 July 2002