Welcome to the C-more Micro Programming Software
Version 2.50 Build 00.00 (9 December 2009)
------------------------------------------------------------------------------
This document describes some of what's new in this release of the C-more Micro 
Programming Software. It also includes known issues as well as updated 
information for the documentation provided with this software. The information 
in this file and in the Help system is more up-to-date than that in the manual.


		Contents

	 1. Welcome 							
	 2. Getting Started
	 3. What's New?
	 4. Known Issues
	 5. Technical Support Procedures.
	 6. Documentation Changes.
	 7. Help File Changes.
	 8. Known Problems and Conditions.
	 9. Uninstalling the C-more Micro Programming Software.
	10. Contact Technical Support



Part 1: Welcome

AutomationDirect.com would thank you for using the C-more Micro Programming 
Software. We have loaded many powerful and exciting features to the New C-more 
Micro software; however we know that our customers sometimes have great ideas 
for features. Please feel free to give us input on the C-more Micro product 
line and you may even request features that you feel would add more value to 
the software for your application

Part 2: Getting Started

See the C-more Micro Programming Software Installation Guide for help on 
installing the software on your PC. Also, see the Hardware Quick Start 
guide that comes with every panel. You can find the same information in 
the C-more Micro help files by selecting the Getting Started item under the 
Help menu of the C-more Micro Programming Software window.


Part 3: What's New?


12/9/2009 Version 2.50 Build 00.00

New features
1. Support for  new 6 TFT 32K color panel, EA1-T6CL.
2. Addition of 'Multi-State Bitmap' object.
3. Addition of advanced 'Numeric Entry' and 'Numeric Display' options for using Windows Fonts.
4. Updates to the simulator including simulate function keys and numeric keypad bezels.

Improvements: 
1. Modbus RTU driver: allow Registers per Message and Coils per Message to be unique settings per devices
2. Modbus RTU driver: add "2" as an option in the "Registers Per Message" field for the Panel Manager settings
3. COM port selection - add "Detail" button to all COM port selections

Bug Fixes
1. Panel beep does not work after password screen (when using PLC to Panel option)
2. Entivity Modbus RTU, Discrete Objects are not updated on the screen.
3. Bar Graph Object using "Target Line" option does not work.
4. 3 inch panel system screen displays incorrect memory information
5. Message Database Export Problem


6/2/2009 Version 2.31 Build 00.00


  Bug Fix (from the current Ver.2.30.0.0)

1. Panel Locks up when using the CLICK PLC Driver and pressing the F1+F5 keys to access System Screen



5/27/2009 Version 2.30 Build 00.00

Improvements: (from the current Ver.2.20.0.0)
1. Improvement for beep sound behavior.
2. Numeric Entry - Add "Clear Entry" selection - that clears the entry field when keypad opens.  Default = deselected
3. AB Enhancements (Add Long data type, String data type and Allen Bradley CSV import)
4. Function Key LED - Eliminate or reduce the blink time when changing screen
5. Limit C-more Tag data type selection for Allen-Bradley data type combinations

  Bug Fix (from the current Ver.2.20.0.0)
1. Siemens PPI, Problem with Recipe using 32 bit tags.
2. csv files created when the Windows Regional setting is somewhere other than USA use semicolon to separate fields
3. CSV import differences between C-more and C-more Micro
4. Dynamic Bitmap object does not display 1-pixel-wide bitmap properly
5. Simulation problem: AB drivers (DH485 and DF1), Timer/Counter .ACC/.PRE does not work in Simulation on PC
6. Numeric Display object appears to allow font to be larger than 32x32 but panel displays as 32x32
7. Windows font smoothing option is cleared by Micro software
8. Message Database allows too many embedded tags.


12/16/2008 Version 2.20 Build 00.00
	New Driver Support:
	- Mitsubishi FX-1N(c)/2N(C)/3U(C) (CPU)

	Bugs Fixed:
	1) Read Only Project File - Will not transfer to panel
	2) Protected Project can not be Transferred if objects are overlapping
	3) C-more Micro Import Tag Database is less capable than C-more
	4) Regional Language Settings - Dutch - Causing Error '5000.'?????????


10/22/2008 Version 2.1 Build 00.01		
	Bugs Fixed:
	1) PTC-015 error associated with Vista error "KERegServer.exe not found" 
	2) Indicator Light - Inverse for ON and Normal for OFF - Text is not visible

10/15/2008  Version 2.1 Build 0.0
      New Driver Support:
      - AutomationDirect CLICK
      - Mitsubishi Q/QnA series

	Bugs Fixed:
	Sharing violation EA_.mdb when saving project file

7/2/2008 - Version 2.0 Build 0.0

	New Hardware: 
	1) C-more 6" Micro Panels
	
	- EA1-S6ML
	- EA1-S6MLW

	2) C-more 6" Micro Bezels
		
	- EA-MG6-BZ2
	- EA-MG6-BZ2P

	New Features:
	1) Support for up to 16 alarms	
	2) Line Graph Object
	3) Real Time Graph Object
	4) Analog Meter Object
	
	Improvements:
	- New Numeric Entry Object Style 3 - Style 3 requires an optional keypad bezel.
	- Enhanced labeling of the function key object for 6" panels.
	- Microsoft Vista compatiblity.


	Bugs Fixed:
	- Panel to PLC tags do not map correctly in the simulator.
	- Tag Name Export to XLS creates an extra quote character on tags beginning with a number.
	- EA-MG-SP1 RXD status LED does not light.
	- Export Screen Image with Object Name does not include object name.
	- Bar Graph Object does not display actual value.
	- Numeric Display Object and Numeric Entry Object do not make Fractional number of Digits selection unavailable when Use Tag for Decimal Point is selected.
	- 'Loop Back Test' and 'PLC Enquiry Test' are not displayed correctly.
	- GE SNPX driver: Please allow the I, Q, AI, AQ data types to be Read/Write

3/12/2008 - Version 1.50 Build 8.11

	New Hardware: 
	1) C-more Micro High Contrast White Screen Models
		
	- EA1-S3MLW
	- EA1-S3MLW-N

	New Features:
	1) New Driver Support:
		- Allen-Bradley DH485
		- Siemens S7-200 PPI	
	2) Additional Fonts
		- 32x16 
		- 32x32		
	
	Improvements:
	- Bar Graph - Target Line Added

       Bugs Fixed:
	- Screen Password Entry - While entering a screen password, the password characters are visible.
	- Floating Point - floating value in C-more Micro is different from Floating Point value in the PLC.
	- Import Tagname Database - Tags will not import into C-more Micro if comma is missing at end of line
	- Graphic Library - Add Graphic to Graphic Library DialogBox Broke
	- Frames different between C-more Micro Panel and Programming Software.
	- Bar Graph - Floating Point setting alway changes back to 1 when closing the configuation dialog box and reopening
	- Project Memory Size calculation error
	- Function Object - Function Labels displaying text that was defined for other screens


10/17/2007 - Version 1.2 Build 7.40

	New Features:
	1) New Driver Support:
		- GEFanuc SNPX supports VersaMAx, VersaMax Micro, Micro 90		

	Improvements:
	- Increase available SRAM for increased number of tags by 4 times

	Bugs Fixed:
	- Numeric Entry - Simulator and Panel act differently whe entering numbers
	- Blank Green Screen - Required F2-F4 Reset factory defaults to clear
	- Project Option - does not keep the Backup/Save settings
	- Tag Name Import from Directsoft - spaces not allowed
	- Numeric Display - SW does not display the position of values properly

8/15/2007 - Version 1.2 Build 7.24

	New Features:
	1) New Driver Support:
		- GEFanuc 90/30 SNPX
		- OMRON Host Link Adapter
		- OMRON FINS Serial
		- Mitsubishi FX
		- Think & Do Modbus
		- Touch Panel Test
	2) Touch Panel Test on SETUP MENU

	Improvements:
	- File format and Check sum enhancement for EEPROM Failures; To Prevent Green Blank Screen
	- Changed Protocol Name Text in panel to 2 lines to make more readable

	Bugs Fixed:
	- Screen change pushbuttons are getting cut off in panel but look normal in software
	 
	New Error Codes:
	Error Code	Error Message 		Cause

 	R005		Panel Check Sum Error.  System Info. check sum failed.
 				Panel Info (Not Project) will be initialized.
 
	R006		SW Ver. Mismatch		Software version does not match 
			Use software Ver.xx.xx 				the panel FW version when transferring the project.

5/3/2007 - Version 1.12 Build 7.15A

	Bugs Fixed
	- Shape Objects not displaying on panel

4/16/2007 - Version 1.12 Build 7.15
	
	New Features
 	- Add New Object - Scroll Text (128 Char)
	- Add New feature  Dynamic Text has Scroll Text Option (40 char)
	- Add New feature  Lookup Text has Scroll Text Option (128 char)
       - Add New feature  All PLC drivers support Multiple PLC Node connection on EA-MG-SP1 Port 2

	Improvements
	- Support Internal Tags on the panel (PLC Address Not Required)
	- Improved Touch / Key response
	- Improved performance when communication error occurs
	- Built-in Serial Port 1 becomes a dedicated programming port when EA-MG-SP1 Port 2 is configured. (Project can be downloaded with pressing F1 and F5 in this mode)
	- Error PTC-019 : No project File in Panel added (when trying to read project from panel with only the runtime loaded)
	- Display Hourglass instead of message Loading Screen and delay time is adjustable with Setup Screen

	Bugs Fixed
	- Momentary Pushbutton Delaying Shutting Off
	- Indicator Button and Bitmap Button do not work properly if "Indicator Tag Name" and "Push Button Tag Name" has the same address number, i.e.X0 and Y0 respectively.

2/14/2007 - Version 1.11 Build 6.51B

	Full Release - 	Firmware change only:

	- "Sticky" Momentary Pushbutton
	- When using Koyo Modbus and Panel<-> PLC, "Send Current Key Status", Panel can lockup when a function key is pressed.

1/11/2007 - Version 1.11 Build 6.51A

	Firmware release only:

	- Corrected a periodic PLC Timeout associated with DL 06 and 260 PLC's.
	- Corrected Problem using Momentary Pushbutton with PLC <-> Panel functions such as screen change.
	- Fixed Panel lockup associated with pressing the function keys and bezel buttons too quickly.

12/18/2006 - Version 1.11 Build 6.51

		1) Support Allen Bradley DF1 for Micrologix, SLC500, PLC5
		2) Increment and Decrement Added to Function Key Options
		3) Various Bug Fixes

		General

		1) Lookup Text Justification Issue Corrected
		2) Corrected Screen Selector allows Non-existing screens to be added to the list, locks up panel
		3) Corrected Panel Freezing while using Tab Index Function
		4) Corrected BCD Data Type Display Issue
		5) Corrected Panel switching to User Screen on it own while in System Screen.


		Touch Screen

		1) Fixed Panel Missing Touches to screen or Key Strokes on Function and Bezel Keys

09/18/2006 - Original Release C-more Micro Programming Software 
             Version 1.1 Build 6.39





Part 4: Known Issues

Screen DPI settings: It is recommended that when using C-more Micro Programming
software, the DPI setting should be one of the following settings:
     72dpi (75%)
     96dpi (100%)
    120dpi (125%)
    144dpi (150%)
    192dpi (200%)
Failure to do so will cause text in a project to display incorrectly. 

USB-to-Serial Drivers: It is recommended to disconnect any USB devices except 
mouse and keyboard during installation. Some USB devices can interfere with the installation and uninstallation of the Koyo USB to serial driver.

We request that you contact us with any Issues that 
you might find via fax (1-770-886-3199) or inquiry at 
http://support.automationdirect.com/techinquiry.html.


Part 5: Technical Support Procedures

If you need technical assistance, you may find the information you need on our web site at www.automationdirect.com/support. If you prefer, you can send us your inquiry at http://support.automationdirect.com/techinquiry.html.Or you may call Automationdirect at 1-770-844-4200 -- our technical support team is available to answer your questions weekdays from 9 AM - 6 PM EST. Or you can fax the information to us at 1-770-886-3199 any time of day.

Please provide the Version information when requesting technical support. You'll 
find it under the Help/About C-more Micro Programming Software Version.


Part 6: Documentation Changes

We request that you contact us with any corrections, enhancements, changes that you would like to see in the documentation via fax (1-770-886-3199) or inquiry at http://support.automationdirect.com/techinquiry.html.

Please always check the On-Line Help files and our web site at 
www.automationdirect.com/support for updated and new information.


Part 7: Help File Changes

Refer to the "What's New" Topic in the Help File for a list of changes and additions to the help file.

We request that you contact us with any corrections, enhancements, changes that you would like to see in the documentation via fax (1-770-886-3199) or inquiry at http://support.automationdirect.com/techinquiry.html

Please always check the On-Line Help files and our web site at 
www.automationdirect.com/support for updated and new information.


Part 8: Known Problems and Conditions

Find a Problem?
Please check the version of your Windows once again.
C-more Micro Programming Software runs under the following Windows Operating systems: 
Windows XP Pro/XP Home with SP2, Windows 2000 with SP4, and Windows Vista (32 bit)

Please report any problems to Automationdirect via 
http://support.automationdirect.com/techinquiry.html  or by calling 1-770-844-4200.


Part 9: Uninstalling C-more Micro Programming Software

Before Starting: Data Backup
If you have saved projects that you feel are important to you, then you will need to make a backup of these files. Please backup your files such as Project files and Library files before uninstalling.

Before Starting: Remove USB Cable
If the C-more Micro Panel is connected to the PC USB port via the USB-Serial 
Converter (EA-MG-PGM-CBL), then the USB driver will be active. Please Remove USB Cable between PC and C-more Micro panel before Uninstalling. It is also recommended to disconnect any USB devices except mouse and keyboard. Some USB devices can interfere with the installation and uninstallation of the Koyo USB to serial driver.


Part 10: Contact Technical Support

Our technical support hours are from 9am to 6pm Eastern Standard Time Monday 
through Friday.

Telephone: 1-770-844-4200
FAX: 1-770-886-3199

Technical Support Inquiry
http://support.automationdirect.com/techinquiry.html

Discussion Forum: AutomationDirect Customer Forum
http://forum1.automationdirect.com/

-----------------------------------------------------------------------------------
Copyright (C) 2004 - 2009 AutomationDirect and KOYO ELECTRONICS INDUSTRIES CO., LTD. and WinSystem Co., Ltd. All Rights Reserved.