Latest shipping version:
Recent Firmware History:
Version: 1.2.10.9
Details:
Version: 1.2.7.66
Details:
P3-530
Firmware 1.2.7.66
Release Date: January 22nd, 2021
Bugs fixed:
1.) This firmware modification resolves a factory test issue and should have no impact on customer applications.
Version: 1.2.7.65
Details:
P3-530
Firmware 1.2.7.65
Release Date: September 17th, 2020
Bugs fixed:
1.) Modbus TCP Server. When writing a block of mixed 32-bit and 16-bit integers
to the PLC, the data can get written to the wrong location and return an illegal
data address exception in certain situations
Version: 1.2.7.39
Details:
Release date: 6/10/19
Bugs fixed:
1.) CPU may lockup with serial Modbus instructions when transitioning Run-Stop.
Version: 1.2.7.37
Details:
Release date: 12/12/18
Improvements:
1.) Added support for new features:
a. Secure integrated Email
b. Network Time Service
c. Domain Name Server
Bugs fixed:
1.) Modbus RTU, as slave, does not show exception for unknown Function Codes.
2.) CPU date not changing correctly if set to some older time frames.
3.) First containing ModBus/TCP non-existing devices in call task takes 2x longer than subsequent scans.
4.) Retentive data backup behavior does not complete as user specification if set to minimum.
Version: 1.1.15.114
Details:
Version: 1.1.15.114
Details:
P3-530 Release Notes
Firmware 1.1.15.114
February 13, 2018
Bugs fixed:
1) Digital Inputs may not be available on first scan for the local base or any remote bases set to local.
Version: 1.1.15.111
Details:
Release Date: January 3rd, 2018
Hardware:
1) Support for new USB chip on P3 backplanes.
Bugs fixed:
1) Mitigate effects on CPU when the external Ethernet port on the CPU experiences irregular Ethernet traffic.
Version: 1.1.15.108
Details:
Bugs fixed:
1.) System discovery and project transfer fails resulting in E01201 Sema Obtain error. This may happen when on a network with other devices using broadcast messages.
2.) Repeated consecutive power cycles may force CPU to stop mode and corrupt NAND flash.
Version: 1.1.15.104
Details:
P3-530
Firmware 1.1.15.104
Bugs fixed:
1.) Incurring drop packets during project transfer via Ethernet may cause the transfer to fail.
Version: 1.1.15.101
Details:
Bugs fixed:
1.)When using a P3-SCM module with CPI/CPO instructions a stop mode transfer can cause the P3-530 to stop communication to the SCM and create an E1005 error.
Version: 1.1.15.99
Details:
P3-530 Release Notes
Firmware 1.1.15.99
November 10, 2014
Bugs fixed:
1.)Data Logging .csv files can lose data after a power cycle.
2.)Any Data Logging file created since last power up cannot be deleted by the web server.
3.)Web server may cause possible E01005 ‘System Restart’ error.
Version: 1.1.15.98
Details:
P3-530 Release Notes
Firmware 1.1.15.98
September 29, 2014
Bugs fixed:
1.) Quick disconnect and reconnect from Modbus Master device(s) may cause PAC E01005 System Restart error.
Version: 1.1.15.97
Details:
Version: 1.1.14.39
Details:
FW 1.1.14.39 Release Notes
December 17, 2013
Bugs
1)After upgrading FW to 1.1.14.38 the serial com port settings reset to default.
Version: 1.1.13.24
Details:
FW 1.1.13.24 Release Notes
June 17, 2013
Improvements
1) Increase multicast TTL default to 30.
2) Web Server page support for new system tags along with behavior check
First Scan Interval [x100=usec] SWR-001530
Portable Memory Device Ready SBR-000001
Portable Memory Device Eject SBRW-001006
Bugs
1) Extended Modbus reply to block requests of 2 dimension arrrays of BCD16 and BCD32 data types are wrong.
2) P3-CPU Enet interface becomes invalid if set up improperly (such as 255.255.255.255 or 127.0.0.1)
3) Repair DHCP functionality.
4) P3-CPU(P3-550 Rev. D) fail to download the 2nd base firmware along with the certain size of the PAC project.
5) Portable Memory Device Ready bit stays on after power down and removal of usb device.
6) Portable Memory Device Ready bit not initialized correctly when an invalid value is passed to it.
Version: 1.1.13.17
Details:
Initial launch firmware