AutomationDirect logo Firmware Revisions for D0-DCM



Latest shipping version:

 

Recent Firmware History:


Version: V1.10
Details:
*** Important ***
To use this D0-DCM firmware, please make sure the DL05 and DL06 have the following firmware.

DL05: V5.30 or newer
DL06: V2.40 or newer

[Fixed problems]
- RW, WX: When the D0-DCM is installed in a DL05, the RX and WX instructions do not work correctly with the D0-DCM Port 2.
- MWX: When the D0-DCM is installed in a DL06, the MWX instruction does not work correctly in the single coil mode with the D0-DCM Port 2.
- PRINT: When the D0-DCM is installed in a DL05, the PRINT instruction does not work with the D0-DCM Port 2.
- PRINT: When the D0-DCM is installed in a DL06, the PRINT instruction does not work with the D0-DCM Port 2 (RS-422). RS-232 works correctly.
- AIN: When the D0-DCM is installed in a DL06, the AIN instruction does not work correctly with the D0-DCM Port 2.