AutomationDirect logo Firmware Revisions for C-More Micro



Latest shipping version:

 

Recent Firmware History:


Version: 2310000
Details:
Bug Fix (from the current Ver.2.30.0.0)

1. Panel Locks up when using the CLICK PLC Driver and pressing the F1+F5 keys to access System Screen


Version: 2300000
Details:
See the Release Notes for more details:

http://support.automationdirect.com/products/cmoremicro.html

Improvements:
1. Improvements for beep behavior. See the Release Notes for details.
2. Numeric Entry - Add "Clear Entry" selection - that clears the entry field when the keypad opens.
3. Allen Bradley driver support enhancements (Add Long data type, String data type and Allen Bradley CSV import)
4. Function Key LED - Eliminate or reduce the blink time when changing screen
5. Limit C-more Tag data type selection for Allen-Bradley data type combinations

Bugs Fix (from the current Ver.2.20.0.0)
1. Siemens PPI, Problem with Recipe using 32 bit tags.
2. csv files created when the Windows Regional setting is somewhere other than USA use semicolon to separate fields
3. CSV import differences between C-more and C-more Micro
4. Dynamic Bitmap object does not display 1-pixel-wide bitmap properly
5. Simulation problem: AB drivers (DH485 and DF1), Timer/Counter .ACC/.PRE does not work in Simulation on PC
6. Numeric Display object appears to allow font to be larger than 32x32 but panel displays as 32x32
7. Windows font smoothing option is cleared by Micro software
8. Message Database allows too many embedded tags.


Version: 2200000
Details:
This version adds support for a new Mitsubishi driver for the FX series 1N(C)/2N(C)/3U(C) CPUs.

Bugs Fixed:
1. Read Only Project File - Will not transfer to panel
2. Protected Project can not be transferred if objects are overlapping
3. C-more Micro Import Tag Database is less capable than C-more
4. Regional Language Settings - Dutch - Causing Error '5000.'?????????
Please review the README file that comes with the software for more details.


Version: 2000000
Details:
This is Full Release. Firmware File is available with Software Download Only.

New Hardware:
1) C-more 6” Micro Panels
- EA1-S6ML
- EA1-S6MLW

2) C-more 6" Micro Bezels
- EA-MG6-BZ2
- EA-MG6-BZ2P

New Features:
1) Support for up to 16 alarms
2) Line Graph Object
3) Real Time Graph Object
4) Analog Meter Object

Improvements:
- New Numeric Entry Object Style 3 - Style 3 requires an optional keypad bezel.
- Enhanced labeling of the function key object for 6" panels.
- Version 2.0 is Microsoft Vista compatible.

Bugs Fixed:
- Panel to PLC tags do not map correctly in the simulator.
- Tag Name Export to XLS creates an extra quote character on tags beginning with a number.
- EA-MG-SP1 RXD status LED does not light.
- Export Screen Image with Object Name does not include object name.
- Bar Graph Object does not display actual value.
- Numeric Display Object and Numeric Entry Object do not make Fractional
number of Digits selection unavailable when “Use Tag for Decimal Point” is selected.
- 'Loop Back Test' and 'PLC Enquiry Test' are not displayed correctly.
- GE SNPX driver: Please allow the I, Q, AI, AQ data types to be Read/Write


Version: 1500811
Details:
This is a Full Release. Firmware File is avalilable with Software Download Only

New Hardware:
1) C-more Micro High Contrast White Screen Models
- EA1-S3MLW
- EA1-S3MLW-N

New Features:
1) New Driver Support:
- Allen-Bradley DH485
- Siemens S7-200 PPI

2) Additional Fonts
- 32x16
- 32x32

Improvements:
- Bar Graph - Target Line Added

Bugs Fixed:

- Screen Password Entry - While entering a screen password, the password characters are visible.
- Floating Point - Floating point value in C-more Micro is different from Floating Point value in the PLC.
- Import Tagname Database - Tags will not import into C-more Micro if comma is missing at end of line
- Graphic Library - Add Graphic to Graphic Library DialogBox Broke
- Frames different between C-more Micro Panel and Programming Software.
- Bar Graph - Floating Point setting always changes back to 1 when closing the configuation dialog box and reopening
- Project Memory Size calculation error
- Function Object - Function Labels displaying text that was defined for other screens


Version: 1200740
Details:
10/17/2007 - Version 1.2 Build 7.40

New Features:

1) New Driver Support:
- GEFanuc SNPX supports VersaMAx, VersaMax Micro, Micro 90
Improvements:
- Increase available SRAM for increased number of tags by 4 times

Bugs Fixed:
- Numeric Entry - Simulator and Panel act differently whe entering numbers
- Blank Green Screen - Required F2-F4 Reset factory defaults to clear
- Project Option - does not keep the Backup/Save settings
- Tag Name Import from Directsoft - spaces not allowed
- Numeric Display - SW does not display the position of values properly


Version: 1200724
Details:
Full Release

New Features:

1) New Driver Support:

- GEFanuc 90/30 SNPX
- OMRON Host Link Adapter
- OMRON FINS Serial
- Mitsubishi FX
- Think & Do Modbus
- Touch Panel Test

2) Touch Panel Test on SETUP MENU

Improvements:
- File format and Check sum enhancement for EEPROM Failures; To Prevent Green Blank Screen
- Changed Protocol Name Text in panel to 2 lines to make more readable

Bugs Fixed:
- Screen change pushbuttons are getting cut off in panel but look normal in software


Version: 02010001
Details:
This is Full Release. Firmware File is available with Software Download Only.

Bugs Fixed in ver 2.1.00.01:
1) PTC-015 error associated with Vista error "KERegServer.exe not found"
2) Indicator Light - Inverse for ON and Normal for OFF - Text is not visible

New Driver Support (available in ver 2.1.0.0):
- AutomationDirect CLICK
- Mitsubishi Q/QnA series

Bugs Fixed in ver 2.1.0.0:
Sharing violation EA_.mdb when saving project file


Version: 02010000
Details:
This is Full Release. Firmware File is available with Software Download Only.


New Driver Support:
- AutomationDirect CLICK
- Mitsubishi Q/QnA series

Bugs Fixed:
Sharing violation EA_.mdb when saving project file


Version: 01120715 A
Details:
Full Release

Bugs Fixed

- Shape Objects not displaying on panel


Version: 01120715
Details:
Firmware version is shipping with the present software release; 1.12 Build 7.15 downloadable from the website at:

http://support.automationdirect.com/products/cmoremicro.html

The firmware is only available with the software download.

Features and Improvements added to this release are:

New Object - Scroll Text (128 Char)
New feature - Dynamic Text has Scroll Text Option (40 char)
New feature – Lookup Text has Scroll Text Option (128 char)
New feature – Support Multiple PLC Node connection on EA-MG-SP1 Port 2
Support for Internal Tags on the panel (PLC Address Not Required)
Display Hourglass instead of “Loading Screen” message


Version: 01110651B
Details:
This firmware release corrects:

- "Sticky" Momentary Pushbutton

- When using Koyo Modbus and Panel<-> PLC, "Send Current Key Status", Panel can lockup when a function key is pressed.

Unzip the file to the \C-more Micro\Firmware folder and use the C-more Micro programming software to update the firmware in your panel.


Version: 01110651A
Details:
This firmware release corrects:

- a periodic PLC Timeout associated with DL 06 and 260 PLC's.
- "Sticky" Momentary Pushbutton bug.

- Panel lockups associated with pressing the function keys and bezel buttons too quickly.

Unzip the file to the \C-more Micro\Firmware folder and use the C-more Micro programming software to update the firmware in your panel.


Version: 01110651
Details:
Firmware version is shipping with the present software release. This version includes Allen Bradley DF1 protocols for Micrologix, SLC and PLC5 along with updated Help Files. This release also corrects a few miscellaneous bugs. Please review the README file that comes with the software for more details.

Unzip the file to the \C-more Micro\Firmware folder and use the C-more Micro programming software to update the firmware in your panel.


Version: 01010639
Details:
Initial Release