AutomationDirect logo Firmware Revisions for C-More



Latest shipping version:

 

Recent Firmware History:


Version: 2.53
Details:
Version 2.53 corrects an issue with version 2.52 that could cause a panel to freeze with a white screen.


Version: 2.51
Details:
Available as part of software download, firmware is not available independent of software.
8/19/2009 – Version 2.51
New drivers
1) GS Drives Modbus Serial
2) GS Drives Modbus Ethernet

Bugs fixed
3) MultiState Text Indicator, bug when using String Tags
4) Simulation problem: AB drivers (DH485 and DF1), T4:11.ACC does not work in Simulation on PC
5) EZTouch Conversion - Modbus and Modbus TCP - Poll time is not converted properly
6) Alarm message object does not update properly on a Background screen
7) DF1 Half Tag-Based, problem when using two devices of same protocol.
8) Message database doesn't properly display edited message
9) Sounds Crackling on second loop
10) LCD remains dark after screen saver is deactivated by touching the screen in EA7-S6M(-R) panels
11) A-B Ethernet/IP 1100 with two PLCs, problem when communications lost to one PLC.
12) Slider object: Enter and Cancel buttons do not appear when object is narrower than default and On Demand is selected
13) EtherNet/IP Tag Based Control/CompactLogix: Tag Copy of Strings with an odd length does not copy correctly
14) C-more USB Pen Drive Recognition

Readme errata
Version 2.40 item 8 has been changed to read: The total quantity of screens in the project is increased to 9999, limited by available memory.

Improvements
15) Adjust Screen value set by Adjust Screen object should be retentive
16) Event Manager - Tag Event - for Analog Tags, base the event on <, = or > or not equal or like the Visibility option on most objects
17) Line Trend Graph and PID Trend graph Objects - Scroll Buttons - Add Check Box option "Display Scroll Buttons" to Options Tab, Default = checked
18) Modbus RTU & Modbus TCP: Allow write function code for registers and Coils to be selected
19) Radio Button - Expand the object to use the entire 16 bit word instead of just 8 bits.
20) Radio Button - Background to Buttons should be editable
21) Trend Data Logging - CSV file needs headers
22) Event Manager Export/Import - There is a field at the bottom of an Event Manager Export that we can not see. But if it is deleted or if data is added after it on the spreadsheet, the import will not work as expected. Identify this row so it will not be deleted.
23) Limit C-more Tag data type selection to Allen Bradley PLC memory type
24) Modbus RTU and Modbus TCP: Add "2" as an option in the "Registers Per Message" field for the Panel Manager settings
25) Modbus RTU and TCP: allow Registers per Message and Coils per Message to be unique settings per devices
26) Add Numeric/Text Entry Object Focus option
27) Add Byte Swap option in event manager Tag and Tag Copy events for ASCII data.


Version: 2.42
Details:
The Source Data becomes corrupted in the Recipe Object using Single Source Recipe in various circumstances.

This only happens when converting projects from versions older than 2.40 to version 2.40 or 2.41.


Version: 2.41
Details:
Projects from previous versions that are upgraded to version 2.41 will have the Remote Access Feature set to off by default.


Version: 2.40
Details:
In order to make use of the Remote Access feature when upgrading fw the customer must Reset to Factory Default at the panel (this writes new html files)

This version adds the Remote Access Feature.
Also, sample projects install in the Project folder, SMTP authentication support and the option to identify screens with numbers up to 9999 (quantity of screens remains 999)


Version: 2.23 + Service Pack 1
Details:
Bugs Fixed

1) Allen Bradley L5K Import with TagName the same as DataType causes C-more S/W to crash.
2) When Importing over 30,000 tags the Error Message text is wrong.
3) C-more importing Analog I/O Aliases in ControlLogix driver L5K import with wrong data type.
4) Import Message Database with Message Overwrite, Message Text is deleted.


Version: 2.23
Details:
The Firmware is packaged with C-more Programming Software version 2.23 and can not be downloaded separately.

Go to the software download page to download the latest version of the software and to see details of the new features with this release.
http://support.automationdirect.com/products/cmore.html



Version: 2.20 + SP1
Details:
The Firmware is packaged with C-more Programming Software version 2.2 and can not be downloaded separately.

Go to the software download page to download the latest version of the software and to see details of the new features with this release.

http://support.automationdirect.com/products/cmore.html


Version: 2.2
Details:
07/31/2008 - Version 2.2

The Firmware is packaged with C-more Programming Software version 2.2 and can not be downloaded separately.

Go to the software download page to download the latest version of the software and to see details of the new features with this release.

http://support.automationdirect.com/products/cmore.html


Version: 2.1
Details:
04/29/2008 - Version 2.1

The Firmware is packaged with C-more Programming Software version 2.1 and can not be downloaded separately.

Go to the software download page to download the latest version of the software and to see details of the new features with this release.

http://support.automationdirect.com/products/cmore.html



Version: 2.0.7.35E
Details:
Special Firmware Release

There is no need to download this firmware unless you have experienced the problems that are corrected by this release.

For the latest version of the C-more Software, go to the software download page to download the latest version of the software and to see details of the new features with this release.

http://support.automationdirect.com/products/cmore.html

These firmware fixes will be included in the next Full Release of the C-more Software.

Bugs Fixed in the special Firmware Release:

1) Bar Graph not always updating with current PLC data
2) Line length animation not changing as expected


Version: 2.0.07.35B
Details:
Special Firmware Release

There is no need to download this firmware unless you have experienced the problem that is corrected by this release.

For the latest version of the C-more Software, go to the software download page to download the latest version of the software and to see details of the new features with this release.

http://support.automationdirect.com/products/cmore.html

This firmware fix will be included in the next Full Release of the C-more Software

Bug Fixed in the special Firmware Release

Allen Bradley Control/CompactLogix PLC's

EtherNet/IP and DF1


1) Only the first element of REAL ARRAY Tags will update


Version: 2.0.07.35
Details:
09/5/2007 - Version 2.0 Build 07.35

Bugs Fixed
1) False Allen Bradley EtherNet/IP PLC-011 error
2) No * when entering Screen Password


Improvements

1) Retentive Tag Startup Performance Improved
2) Added Copy and Paste of Individual Records within Event Manager


Version: 2.0.07.35
Details:
09/5/2007 - Version 2.0 Build 07.35

Bugs Fixed
1) False Allen Bradley EtherNet/IP PLC-011 error
2) No * when entering Screen Password


Improvements

1) Retentive Tag Startup Performance Improved
2) Added Copy and Paste of Individual Records within Event Manager


Version: 2.0.07.32
Details:
Firmware is packaged with software version 2.00 Build 7.32.

Go to the software download page to download the latest version of the software and to see details of the new features with this release.

http://support.automationdirect.com/products/cmore.html

Allen Bradley ControlLogix/CompactLogix Ethernet IP Tag Based Client
Allen Bradley ControlLogix/CompactLogix DF1 Full Duplex Tag Based Client
Allen Bradley ControlLogix/CompactLogix DF1 Half Duplex Tag Based Client
Allen Bradley SLC5/05 EtherNet/IP Client
Allen Bradley MicroLogix 1100 EtherNet/IP Client
Allen Bradley Net-ENI EtherNet/IP Client


Other Features Added:

Recently Open Files Listed in File Menu
Navigation Paths Memorized Automatically


Version: 1.31.7.27
Details:
Firmware is packaged with software version 1.31 Build 7.27.

Go to the software download page to download the latest version of the software and to see details of the new features with this release.

http://support.automationdirect.com/products/cmore.html


Fixed bugs as listed

1) Popup Window Memory Leak
2) Objects overlapping Text Objects causing objects to not update
3) A-B DH485 did not accept Panel Station number set to 1
4) Old project transferred instead of saved project
5) Firmware updates failures
6) Load Library Fail - Database issue with Windows 2000, missing msvcp60.dll
7) Modbus TCP/IP double requests causing "PLC-499 Error Code 0x0004"
8) Recipe Sheet in Popup window causing an error


Version: 1.30.7.21A
Details:
06/01/2007 - Version 1.3 Build 07.21 - Firmware Release Only

Fixed bugs as listed

1) Memory Leak in Line Trend Graph Object - will cause panel to lock up.

This is a Firmware change only. If 1.30 Build 7.21 is already installed, then simply download firmware version


Version: 1.30.07.21
Details:
Firmware is packaged with software version 1.30 Build 7.21.

Go to the software download page to download the latest version of the software and to see details of the new features with this release.

http://support.automationdirect.com/products/cmore.html


Version: 1.21.6.18K
Details:
This is a firmware update only. There is no Software version associated with this update. Software version 1.21.6.18E is still the latest software version at the time of this release.

This release corrects:

Floating Point Accuracy Bug
Floating Point Data Display Bug with the following Objects
Numeric Display
Numeric Entry
Slider
Bar Meter
PID FacePlate
Analog Meter

Trend Graph Update Bug related to clock adjustments

Download and Unzip the file into the \AutomationDirect\C-more\Firmware folder.

Then in the C-more Software go to the Panel Menu and select Update Firmware to update the firmware in the panel.


Version: 1.21.6.18I
Details:
This is a firmware update only. There is no Software version associated with this update. Software version 1.21.6.18E is still the latest software version at the time of this release.

This release corrects some performance issues related to transparency and bitmaps, especially in the EA7-T12C and EA7-T15C panels.


Version: 1.21.6.18E
Details:
This release corrects an issue with the EA-AC power adapter. The C-more Panel was responding incorrectly to the power loss signal from the power adapter. The panel would go blank for no obvious reason and required a power cycle to recover.


Version: 1.21.6.17
Details:
Firmware is packaged with software version 1.21 Build 6.18A


Version: 1.1.1.3a
Details:
Corrects "Backlight Error"


Version: 1.1.1.3
Details:


Version: 1.1
Details:
Initial shipping version