AutomationDirect Logo Think & Do Software Frequently Asked Questions


Press "Ctrl-F" to search for specific words in this FAQ.


Click here to view all Think & Do Software FAQs with answers on one page.

  1. I just upgraded to T&D 5.0. Now every time I go to run T&D I get "Data Logger Error" (No Runtime is available. Data Logging is not available at this time).
  2. What version of OP-Winedit software do I need in order for my OptiMate panel to communicate with Think & Do?
  3. Can Think & Do PC-based control software be used as a DeviceNet master?
  4. Does Windows 2000 support Think & Do software?
  5. Does the D2-Ctrint work with Think & Do?
  6. Can I use T&D to multiple EBCs?
  7. Is it possible to have Think N Do 5.2 and 6.1 installed on the same PC?
  8. Im using a Think & Do PC and a WINPLC. Can I get DDE info directly from the WINPLC?
  9. What version of Think n Do Live supports Terminator I/O?
  10. I have 2 or more network cards installed in a computer where both are using TCP/IP protocol. I can PING the WinPLC, but cannot connect using ESP.
  11. I'm using Think&Do Live/Studio and I'm trying to connect to an H2/H4/T1H-EBC. But I keep getting errors.I have NetEdit and it can see the EBC with no problems. What could be wrong?
  12. I need to update my WinPLC to Live 5.4, but I can't find the update.bat program or the WinPLC runtime version 5.4 directory specified in the Updating a WinPLC system help procedure.
  13. Does Think & Do or Studio work with Windows Vista?
  14. Is a demo version of Think & Do available?
  15. My ThinknDo Studio, TnD V8.x USB/Parallel key is physically damaged and no longer works. What can I do?
  16. Where can I find more support information for TnD or Studio?
  17. Where can I get the manual for TnD V8 ?
  18. TnD doesn't find my Setinel Key. Where can I get Sentinel Key drivers?
  19. Can I upgrade from Studio to TnD V8.x ?
  20. What versions of Think & Do and MS Windows are compatable ?
  21. Conversion notes for Think & Do Version 8.x
  22. How can I enable Counter data types in Think & Do?


Troubleshooting Guides