AutomationDirect Logo Stacklights Frequently Asked Questions


Press "Ctrl-F" to search for specific words in this FAQ.


Click here to view all Stacklights FAQs with answers on one page.

  1. Can you have a Stacklight with one flash and one steady light?
  2. Do you sell the replacement LEDs for the Stacklights?
  3. Do you offer a 4-position switch to control Stacklights?
  4. Can you install a higher wattage bulb in a Stacklight?
  5. Is there any way to use a Triac output with an LED Stacklight without having the problem of Triac leakage?
  6. What is the current draw on the 120 Volt Cutler-Hammer Stacklight Alarm Modules ?
  7. What is the current draw on the 24 Volt Cutler-Hammer Stacklight Alarm Modules?
  8. What is the current draw on the 120 Volt Cutler-Hammer Stacklight Strobe Modules?
  9. What is the current draw on the 24 Volt Cutler-Hammer Stacklight Strobe Modules?
  10. What is the current draw on the 120 Volt Cutler-Hammer Stacklight LED Lamps?
  11. What is the current draw on the 120 Volt Cutler-Hammer Stacklight Incandescent Lamps?
  12. What is the current draw on the 24 Volt Cutler-Hammer Stacklight LED Lamps?
  13. What is the current draw on the 24 Volt Cutler-Hammer Stacklight Incandescent Lamps?
  14. What is the current draw on the 120Volt Cutler-Hammer LED Indicators?
  15. What is the current draw on the 120Volt Cutler-Hammer Incandescent Indicators?
  16. What is the current draw on the 24 Volt Cutler-Hammer LED Indicators?
  17. What is the current draw on the 24Volt Cutler-Hammer Incandescent Indicators & Illuminated Switches?
  18. Where can I find samples of the audio alarms used by the E26 Stacklights?
  19. Can the stacklights be used outdoors?
  20. If I use an alarm module on my stacklight which wiring terminal does the alarm module use?


Troubleshooting Guides