AutomationDirect Logo Process Control Frequently Asked Questions


« Return to the FAQ index

Question How many feet of thermocouple wire can I use?
Answer There is an input limitation of >10Mohms impedance for the PM/TC/PC controllers and >4.7M for the Solo controllers. Review the specifications of the thermocouple wire (diameter, distance, material, etc.) to make a determination of distance limitations. If the environment is electrically noisy or the run exceeds the limitations of the controller, then a transmitter can be used to boost the signal and convert it to a 4-20 ma input (in which case a TC33 cannot be used because of no 4-20 ma input.)

FAQ Subcategory:

This item was last updated on 09-21-2007
Document ID: 926


The information provided in the AutomationDirect knowledge base is provided "as is" without warranty of any kind. AutomationDirect disclaims all warranties, either express or implied, including the warranties of merchantability and fitness for a particular purpose. In no event shall AutomationDirect or its suppliers be liable for any damages whatsoever including direct, indirect, incidental, consequential, loss of business profits or special damages, even if AutomationDirect or its suppliers have been advised of the possibility of such damages. Some states do not allow the exclusion of limitation of liability for consequential or incidental damages so the foregoing limitation may not apply.