AutomationDirect Logo Think & Do Frequently Asked Questions


« Return to the FAQ index

Question I'm using Think&Do Live/Studio and I'm trying to connect to an H2/H4/T1H-EBC. But I keep getting errors.I have NetEdit and it can see the EBC with no problems. What could be wrong?
Answer This problem is usually the result of having 2 NIC( Ethernet) cards installed in the same PC. If this is the case you need to access the network settings of the NICs specifically the Protocols that are assigned to each card. On the NIC that is used for your company you should disable/remove/uncheck the NWLink IPX/SPX protocol if installed. Then on the NIC card that is dedicated to the Think&Do system you should enable/install/check the NWlink IPX/SPX protocol and the TCP/IP protocol. You should also check to make sure that an address has been set on the EBC by toggling at least one dip switch to the ON position.

FAQ Subcategory:

This item was last updated on 01-18-2002
Document ID: 900


The information provided in the AutomationDirect knowledge base is provided "as is" without warranty of any kind. AutomationDirect disclaims all warranties, either express or implied, including the warranties of merchantability and fitness for a particular purpose. In no event shall AutomationDirect or its suppliers be liable for any damages whatsoever including direct, indirect, incidental, consequential, loss of business profits or special damages, even if AutomationDirect or its suppliers have been advised of the possibility of such damages. Some states do not allow the exclusion of limitation of liability for consequential or incidental damages so the foregoing limitation may not apply.