| Question | When I use a relay card for drive control, it seems that my relays stick or do not operate correctly. How can I correct this problem? |
| Answer | Review the minimum load requirements of the PLC card or relays in question. The intelligent terminals of VFDs do not represent a significant load. If the drive's input terminal load does not meet or exceed the minimum requirements of the controller, then additional load will need to be added. A large resistor in parallel is usually the fix to this occurrence. The smaller the relay, the more it is likely to have a minimum load requirement because of contact material and surface area contact. Each relay has a wiping current it must exceed to work properly. The requirements of gold contacts versus silver-tin-oxide contacts are enough to cause a problems in some cases. |
FAQ Subcategory:
This item was last updated on 09-25-2007
Document ID: 890
The information provided in the AutomationDirect knowledge base is provided "as is" without warranty of any kind. AutomationDirect disclaims all warranties, either express or implied, including the warranties of merchantability and fitness for a particular purpose. In no event shall AutomationDirect or its suppliers be liable for any damages whatsoever including direct, indirect, incidental, consequential, loss of business profits or special damages, even if AutomationDirect or its suppliers have been advised of the possibility of such damages. Some states do not allow the exclusion of limitation of liability for consequential or incidental damages so the foregoing limitation may not apply.