AutomationDirect Logo General Drives Questions Frequently Asked Questions


« Return to the FAQ index

Question What is the difference between 208, 220, 230, and 240 VAC systems?
Answer In NA, the terms 220V, 230V, and 240V all refer to the same system voltage level. However, 208V refers to a different system voltage level. In NA the utility companies are required to deliver split phase 240VAC for residential use. That is two 120VAC (+/- 5 %) legs. With electrical loads, the voltage will drop, hence the common reference to voltages below 120 and 240, such as 110, 115, 220, and 230. Very Important: when the drive is hooked up for single phase operation (it is a slight misnomer) L1 has a 120VAC hot and L3 has a 120VAC hot (of opposite polarity), for a total of 240VAC. The manual states that a neutral is used. However, the neutral is only used with European single phase 220 on a single leg. The 208VAC system is not the same as 240VAC. It uses a “Y” style transformer with a neutral, and will yield 208VAC between two phases and 120VAC from hot to neutral. We do not recommend using a corner grounded or midpoint tap grounded “delta” secondary style transformer. The phases are not all balanced; one phase is always tied to ground. The voltage mismatch can negatively infulence the drive's performance.

FAQ Subcategory:

This item was last updated on 09-25-2007
Document ID: 834


The information provided in the AutomationDirect knowledge base is provided "as is" without warranty of any kind. AutomationDirect disclaims all warranties, either express or implied, including the warranties of merchantability and fitness for a particular purpose. In no event shall AutomationDirect or its suppliers be liable for any damages whatsoever including direct, indirect, incidental, consequential, loss of business profits or special damages, even if AutomationDirect or its suppliers have been advised of the possibility of such damages. Some states do not allow the exclusion of limitation of liability for consequential or incidental damages so the foregoing limitation may not apply.