| Question | On the SJ100/L100 when I run multi-speeds, do I need to set A20? |
| Answer | A20 can be considered multi-speed 0, If A01 is set to 02 (internal parameter) the frequency setting will be reached at the initialization of the run enable. E.G. I want the drive to hit 50Hz as soon as the fwd terminal is closed and all other multi-speed terminals are open.
If A01 is set to 01 (terminal) A20 becomes invisible. The first multi-speed will be reached after the fwd is enabled and the terminal assigned to Multi-speed 01 is closed. E.G. I want the drive to be at 0Hz when the fwd terminal is closed and all the other terminals are open. I want the drive to hit 50Hz when both fwd and terminal (multi-speed 1) are closed and all the other terminals are open.
Another look:
Reaction:
o Drive to X Hz at run enable.
Settings:
o A01 |
FAQ Subcategory: None
This item was last updated on 08-23-2001
Document ID: 803
The information provided in the AutomationDirect knowledge base is provided "as is" without warranty of any kind. AutomationDirect disclaims all warranties, either express or implied, including the warranties of merchantability and fitness for a particular purpose. In no event shall AutomationDirect or its suppliers be liable for any damages whatsoever including direct, indirect, incidental, consequential, loss of business profits or special damages, even if AutomationDirect or its suppliers have been advised of the possibility of such damages. Some states do not allow the exclusion of limitation of liability for consequential or incidental damages so the foregoing limitation may not apply.