AutomationDirect Logo General Drives Questions Frequently Asked Questions


« Return to the FAQ index

Question What is ringing and what happens to the motor when I place it more than 50 ft away from the drive with no line reactor?
Answer High voltage ringing (reflective voltage) occurs on all VFD’s. With the advent of IGBT’s replacing SCR’s on smaller more in-expensive drives, it has become more pronounced. It is capacitive coupling effect caused by high speed switching (commutation.) Distance greatly enhances the effect. Cables on the output side of the drive act like capacitors. When the IGBT’s switch or produce the PWM output, the higher frequency part of the current will find a path through that capacitance. Think of the cable being a capacitor that increases in size as the cable length increases. Ringing is very detrimental to motors; it weakens the first stage rotor windings and is detrimental to the life expectancy of a motor. This is especially true for motors under 10 hp, they are machine wound typically, thinner coats of varnish, and have neither phase nor end paper (I.E. aggregate insulation properties.) That’s why we always recommend a drive rated motor. Quality is everything concerning motors. Vintage and non-drive rated motors that are used with VFD’s have a lifespan of unknown proportions. You simply cannot know what to expect from them. Long cable runs with its ringing can also add 10 to 15% of the drive current rating. Therefore, the drive may start to trip out on excessive current. The capacitance will also cause a voltage drop that may cause speed performance problems on the lower end of the speed scale (increased current demand for demanded torque.) A few general guidelines: (1) Try to reduce distances as much as possible (2) Distances of greater than 50 ft (cabled distance not physical distance,) use an output line reactor (3) Always use a drive rated motor.

FAQ Subcategory:

This item was last updated on 02-20-2004
Document ID: 747


The information provided in the AutomationDirect knowledge base is provided "as is" without warranty of any kind. AutomationDirect disclaims all warranties, either express or implied, including the warranties of merchantability and fitness for a particular purpose. In no event shall AutomationDirect or its suppliers be liable for any damages whatsoever including direct, indirect, incidental, consequential, loss of business profits or special damages, even if AutomationDirect or its suppliers have been advised of the possibility of such damages. Some states do not allow the exclusion of limitation of liability for consequential or incidental damages so the foregoing limitation may not apply.