AutomationDirect Logo DL205 Frequently Asked Questions


« Return to the FAQ index

Question Can the DL205 be used on a Modbus network?
Answer The D2-240, D2-250-1 and D2-260 can be used on a Modbus network. The D2-250-1 and D2-260's bottom port can be set to Modbus master/slave. Also, the DCM module can act as a Modbus slave when used with the D2-240 or D2-250 or D2-250-1 or D2-260. The Modbus RTU (hex) protocol is supported. The D2-230 cannot be used on a Modbus network.

FAQ Subcategory:

This item was last updated on 01-08-2004
Document ID: 62


The information provided in the AutomationDirect knowledge base is provided "as is" without warranty of any kind. AutomationDirect disclaims all warranties, either express or implied, including the warranties of merchantability and fitness for a particular purpose. In no event shall AutomationDirect or its suppliers be liable for any damages whatsoever including direct, indirect, incidental, consequential, loss of business profits or special damages, even if AutomationDirect or its suppliers have been advised of the possibility of such damages. Some states do not allow the exclusion of limitation of liability for consequential or incidental damages so the foregoing limitation may not apply.