| Question | I need to add another module to my DL205 9-slot base, but the rack is full. What can I do? |
| Answer | 1.- D2-250-1 and D2-260 are the only CPUs supporting local expansion. You need to change the base D2-09B to D2-09B-1 if this is the case. 2.- You can use ERM/EBC system with all CPUs except D2-230. 3.- A D2-RMSM with a D2-240, a D2-250 and a D2-260, or the bottom port of a D2-250(1) or D2-260 CPU can serve as a remote I/O master. The D2-RSSS serves as the remote slave and resides in the CPU slot of the remote base. Since this is true remote I/O, the scan is handled differently than local I/O.The D2-230 does not support remote I/O. |
FAQ Subcategory:
This item was last updated on 10-06-2003
Document ID: 61
The information provided in the AutomationDirect knowledge base is provided "as is" without warranty of any kind. AutomationDirect disclaims all warranties, either express or implied, including the warranties of merchantability and fitness for a particular purpose. In no event shall AutomationDirect or its suppliers be liable for any damages whatsoever including direct, indirect, incidental, consequential, loss of business profits or special damages, even if AutomationDirect or its suppliers have been advised of the possibility of such damages. Some states do not allow the exclusion of limitation of liability for consequential or incidental damages so the foregoing limitation may not apply.