| Question | Can the DL05 communicate with other DirectLogic PLCs? |
| Answer | Yes, the DL05 can communicate to all of the other DirectLogic PLCs including the DL06, DL105, DL205, DL305 and DL405 families. The DL05 can be a serial master or slave to a DL06 (DirectNet or Modbus RTU), D2-240 (DirectNet)D2-250-1(DirectNet or Modbus RTU), D2-260 (DirectNet or Modbus RTU), D3-340 (DirectNet), D3-350 (DirectNet or Modbus RTU), D4-440 (DirectNet), and D4-450 (DirectNet or Modbus RTU). It can also be an Ethernet master or slave when using an optional Ethernet Communications Module in the option slot of the DL05. An RS232 to RS422/485 converter will be required for communications wiring. |
FAQ Subcategory:
This item was last updated on 12-12-2007
Document ID: 6
The information provided in the AutomationDirect knowledge base is provided "as is" without warranty of any kind. AutomationDirect disclaims all warranties, either express or implied, including the warranties of merchantability and fitness for a particular purpose. In no event shall AutomationDirect or its suppliers be liable for any damages whatsoever including direct, indirect, incidental, consequential, loss of business profits or special damages, even if AutomationDirect or its suppliers have been advised of the possibility of such damages. Some states do not allow the exclusion of limitation of liability for consequential or incidental damages so the foregoing limitation may not apply.