AutomationDirect Logo Sensors Frequently Asked Questions


« Return to the FAQ index

Question Does AutomationDirect offer an AC proximity sensor in a quick-disconnect model?
Answer Yes, the 12mm VM1 and 18mm VK1 series of AC Inductive proximity sensors are available with an M12 4-pin connector. They can be used with the optional 2 meter and 7 meter M12 quick-disconnect cables also offered by AutomationDirect.

FAQ Subcategory:

This item was last updated on 12-07-2007
Document ID: 404


The information provided in the AutomationDirect knowledge base is provided "as is" without warranty of any kind. AutomationDirect disclaims all warranties, either express or implied, including the warranties of merchantability and fitness for a particular purpose. In no event shall AutomationDirect or its suppliers be liable for any damages whatsoever including direct, indirect, incidental, consequential, loss of business profits or special damages, even if AutomationDirect or its suppliers have been advised of the possibility of such damages. Some states do not allow the exclusion of limitation of liability for consequential or incidental damages so the foregoing limitation may not apply.