AutomationDirect Logo General Drives Questions Frequently Asked Questions


« Return to the FAQ index

Question The term "inverter" is a little confusing, since we also use "drive" and "amplifier" to describe the electronic unit that controls a motor. What does "inverter" mean?
Answer The terms inverter, drive, and amplifier are used somewhat interchangeably in industry. But there are subtle differences. A drive can refer to the motor, the control electronics, or both. This term is used particularly when the motor and electronics are integrated in the same housing. The term variable speed drive can include many types of devices - anything that has a variable speed output, which includes the Hitachi inverter. Amplifier more commonly refers to a linear amplifier for servo motor control, or a stepper motor driver IC. Finally, we use inverter to describe the Hitachi motor controller because of the way the switching electronics alternately inverts or directly couples its internal DC voltage bus to generate a variable AC output. The terms AC drive, AFC (adjustable frequency controller), AFD (adjustable frequency drive), ASD (adjustable speed drive), and VFD (variable frequency drive) are also used to describe speed controllers for three phase AC induction motors.

FAQ Subcategory:

This item was last updated on 02-20-2004
Document ID: 284


The information provided in the AutomationDirect knowledge base is provided "as is" without warranty of any kind. AutomationDirect disclaims all warranties, either express or implied, including the warranties of merchantability and fitness for a particular purpose. In no event shall AutomationDirect or its suppliers be liable for any damages whatsoever including direct, indirect, incidental, consequential, loss of business profits or special damages, even if AutomationDirect or its suppliers have been advised of the possibility of such damages. Some states do not allow the exclusion of limitation of liability for consequential or incidental damages so the foregoing limitation may not apply.