« Return to the list of questions
Question
Conversion notes for Think & Do Version 8.x
Answer
Current Think & Do Version 8.x Project Conversion notes. (From the Think & Do Readme.txt file)
The conversion of existing Studio projects (version 7.x) to Think & Do is supported, but with the following limitations/restrictions:
- Requires Visio 2002 to be installed on the system.
- For each user, Visio's macro security level must be set to low. This is automatically done for the one who installs Think & Do, but can also be done by running the "Disable Visio Security" shortcut from the Start Menu's "Phoenix ContactThink & DoMisc" folder.
- All of the logical connections between blocks will be converted, but only the basic set of physical connections will be drawn.
- Live! Capture blocks are unavailable in Think & Do and will therefore be replaced with a Call block as a placeholder.
- The Visio-based HMI screens are skipped/ignored.
Before this conversion though, it is recommended that you do the following to better prepare the Studio project:
- Go to the project folder and delete its "Intermediate"
subdirectory.
- From Studio's ProjectCenter, open the project and choose "Project | Rebuild All" to ensure it is fully up-to-date.
The conversion of existing Live! projects (version 5.x) to Think & Do is also supported, but with the following limitations/restrictions:
- Live! Capture blocks are unavailable in Think & Do and will therefore be replaced with a Call block as a placeholder.
- The HMI screens are skipped/ignored.
FAQ Subcategory: None
This item was last updated on 2014-05-15
Document ID: 1409
The information provided in the AutomationDirect
knowledge base is provided "as is" without warranty of any
kind. AutomationDirect disclaims all warranties, either
express or implied, including the warranties of
merchantability and fitness for a particular purpose. In no
event shall AutomationDirect or its suppliers be liable
for any damages whatsoever including direct, indirect,
incidental, consequential, loss of business profits or
special damages, even if AutomationDirect or its
suppliers have been advised of the possibility of such
damages. Some states do not allow the exclusion of
limitation of liability for consequential or incidental
damages so the foregoing limitation may not apply.