AutomationDirect Technical Support
AutomationDirect | Direct Sales in US and Canada | 1-800-633-0405

C-more Frequently Asked Questions AutomationDirect Logo


« Return to the list of questions

Question

Can you update a project and optionally the firmware using a compact flash card in the built-in CF1 slot of the compact flash capable C-more panels (non -R versions)?

Answer

Yes, you can successfully update a panel project and optionally the firmware using a compact flash card in CF1.
  • You should power down the panel.
  • Insert the compact flash card which has been previously loaded with a copy of the desired project from a PC or another panel into the CF1 slot.
  • Power up the panel.
  • Use the System Screen and the Memory/Restore options to copy the project from the CF1 to the panel. Pick PROJECT to just restore the project, or pick PROJECT and SYSTEM to update the project and the firmware.

There is one extra step. After the update is completed and the panel reboots, power down the panel. Remove the compact flash card. Then re-power the panel in order for the panel to access and run the new project.


FAQ Subcategory: None

This item was last updated on 2021-07-01
Document ID: 1381


The information provided in the AutomationDirect knowledge base is provided "as is" without warranty of any kind. AutomationDirect disclaims all warranties, either express or implied, including the warranties of merchantability and fitness for a particular purpose. In no event shall AutomationDirect or its suppliers be liable for any damages whatsoever including direct, indirect, incidental, consequential, loss of business profits or special damages, even if AutomationDirect or its suppliers have been advised of the possibility of such damages. Some states do not allow the exclusion of limitation of liability for consequential or incidental damages so the foregoing limitation may not apply.


Copyright © 1999- AutomationDirect.com. ALL RIGHTS RESERVED