| Question | How do I adjust the PSD series sensors? |
| Answer | Simplified means to set the PSD25 series pressure sensor. The SET and RESET adjustments (Rings) are mechanically interlocked to prevent setting less than the minimum offset required by the sensor. You cannot use the same pressure setting for the SET and RESET. There must be some hysterisis (offset) to the settings. This is not defeatable. All the directions assume you are looking at the cable end of the sensor. 1. Unlock the sensor adjustments (top most ring). The unlock symbol will line up with center arrow when unlocked. - Rotate the LOCK ring clockwise until it stops. 2. Adjust the SET point (2nd ring from top) to it's lowest setting. - Rotate the SET ring counter-clockwise until it stops. - The RESET ring will start moving at some point to maintain the mimimum offset. 3. Adjust the RESET point (3rd ring from top) to the desired reset point. This is the pressure at which the sensor will turn off after being turned on. This has to be offset from the SET to prevent chattering/rapid cycling. - Rotate the RESET ring clockwise to the desired reset point. - The SET will move also to maintain the offset. 4. Check the setting of the SET ring. You cannot adjust the SET point lower than the reset so the reset may move. - If this needs to be adjusted, the RESET will be affected to maintain the offset. |
FAQ Subcategory:
This item was last updated on 04-08-2009
Document ID: 1187
The information provided in the AutomationDirect knowledge base is provided "as is" without warranty of any kind. AutomationDirect disclaims all warranties, either express or implied, including the warranties of merchantability and fitness for a particular purpose. In no event shall AutomationDirect or its suppliers be liable for any damages whatsoever including direct, indirect, incidental, consequential, loss of business profits or special damages, even if AutomationDirect or its suppliers have been advised of the possibility of such damages. Some states do not allow the exclusion of limitation of liability for consequential or incidental damages so the foregoing limitation may not apply.