| Question | I need to add more IO to my DL06, what are my options? |
| Answer | a. You can use available option modules, such as: discrete IO and/or analog IO, in the four available expansion slots. b. If these are used up, it is possible to use the PLC as master to a second or multiple slave PLCs. You can use a serial or Ethernet connection and use RX/WX instructions to control the IO of other linked PLCs. This is not the preferred method to add IO. c. The end of Chapter 4 in the DL06 user manual covers networking using Modbus RTU or DirecNet protocols. Port 2 on a DL06 supports RS-232, RS-422 and RS-485. Directnet can be used with RS-232 and RS-422. Modbus RTU can be used with the same electrical connections plus it also supports RS-485. d. You should consider using a DL250-1 or DL260 CPU and the engineered local expansion and/or remote IO connections available to that family. Changing the ladder to that family can be as simple as changing the PLC type in the OFFLINE Setup. |
FAQ Subcategory:
This item was last updated on 03-19-2009
Document ID: 1176
The information provided in the AutomationDirect knowledge base is provided "as is" without warranty of any kind. AutomationDirect disclaims all warranties, either express or implied, including the warranties of merchantability and fitness for a particular purpose. In no event shall AutomationDirect or its suppliers be liable for any damages whatsoever including direct, indirect, incidental, consequential, loss of business profits or special damages, even if AutomationDirect or its suppliers have been advised of the possibility of such damages. Some states do not allow the exclusion of limitation of liability for consequential or incidental damages so the foregoing limitation may not apply.