AutomationDirect Logo DL05 Frequently Asked Questions


« Return to the FAQ index

Question Can I read and write data from a second DL05?
Answer a. Yes. You will need to configure one DL05 as the master. The master will use RX and WX instructions to read/write data from the slave units. You can use Modbus or Directnet protocols for this purpose. Either protocol supports multi-drop networks. The following link is to a Master and a Slave ladder example for use with a DL05: (Click here for ladder example). b. Chapter 4 of the DL05 user manual shows: (Click here for Chapter 4). i. Wiring diagrams for a master-slave configuration using RS232 on page 33. ii. Shows how to wire an RS422 network for a master (PC or PLC) to multiple slaves on page 34. iii. Rather than using the F2-UNICON or FA-ISONET depicted in that chapter, use the FA-ISOCON to convert RS-232 to RS-422. The DL05 port 2 only supports RS-232.

FAQ Subcategory:

This item was last updated on 03-12-2009
Document ID: 1167


The information provided in the AutomationDirect knowledge base is provided "as is" without warranty of any kind. AutomationDirect disclaims all warranties, either express or implied, including the warranties of merchantability and fitness for a particular purpose. In no event shall AutomationDirect or its suppliers be liable for any damages whatsoever including direct, indirect, incidental, consequential, loss of business profits or special damages, even if AutomationDirect or its suppliers have been advised of the possibility of such damages. Some states do not allow the exclusion of limitation of liability for consequential or incidental damages so the foregoing limitation may not apply.