| Question | What are the differences between steppers and servos. |
| Answer | Stepper motor control is the most cost-effective way to control a motion but it is an open loop. The accuracy is good if motor is properly sized and the price is reasonable. The torque decreases sharply when the speed increases. Also, the maximum speed for rapid moves and cutting moves are not as high as for servo control. The stepper motors need an amplifier to a train of pulses to deliver current to the windings. The controller is typically a PLC that will generate a speed trapezoidal profile to move the shaft angle from one position to other. There are also dedicated controllers called indexers that will do the same type of pulse generation. Or there are still more sophisticated controllers that can do coordinated motion of several axes. Servo control uses feedback from an encoder to constantly monitor the motion exact position. Modern servos have constant torque over the speed range, and some field weakening only at the top speeds. Using the feedback signals, the control system can correct itself to achieve high speeds and perfect accuracy, even under very strenuous conditions. The modern servos have an amplifier with intelligence to allow several motion types, and can deliver torque, speed or position control with its own intelligence. In any case, a PLC is advisable when there is a need to execute some logic not possible to get from the internal algorithms. |
FAQ Subcategory:
This item was last updated on 03-05-2009
Document ID: 1151
The information provided in the AutomationDirect knowledge base is provided "as is" without warranty of any kind. AutomationDirect disclaims all warranties, either express or implied, including the warranties of merchantability and fitness for a particular purpose. In no event shall AutomationDirect or its suppliers be liable for any damages whatsoever including direct, indirect, incidental, consequential, loss of business profits or special damages, even if AutomationDirect or its suppliers have been advised of the possibility of such damages. Some states do not allow the exclusion of limitation of liability for consequential or incidental damages so the foregoing limitation may not apply.