AutomationDirect Logo Pressure Sensors Frequently Asked Questions


« Return to the FAQ index

Question Can I use the ProSense sensors with gases?
Answer The PTD25(transmitter) models can only be used for gases up to 363 psi. They have an 0-ring that can deteriote with sudden depressurization, and can cause the sensor to fail. For the PSD25(switch) models, they are rated for gas or liquid up to their pressure rating, so long as the chemical compatability is correct. Here are some images of what will happen to the O-ring if sudden depressurization occurs: http://support.automationdirect.com/faq/images/gasket1.png http://support.automationdirect.com/faq/images/gasket2.png

FAQ Subcategory:

This item was last updated on 01-14-2009
Document ID: 1121


The information provided in the AutomationDirect knowledge base is provided "as is" without warranty of any kind. AutomationDirect disclaims all warranties, either express or implied, including the warranties of merchantability and fitness for a particular purpose. In no event shall AutomationDirect or its suppliers be liable for any damages whatsoever including direct, indirect, incidental, consequential, loss of business profits or special damages, even if AutomationDirect or its suppliers have been advised of the possibility of such damages. Some states do not allow the exclusion of limitation of liability for consequential or incidental damages so the foregoing limitation may not apply.