AutomationDirect Logo SureServo Drives and Motors Frequently Asked Questions


« Return to the FAQ index

Question Q: Can I use MODBUS instead of the real digital inputs?
Answer A: Yes, if the firmware of the servo drive is 2.105 or better. This firmware was available around August 2008. Previous versions can do MODBUS but not the digital inputs. The most important parameters are P3-08 and P4-07. P3-08 is a mask that allows defining the physical 8 digital as real or alternatively as virtual, called virtual when used with MODBUS. P4-07 has a dual purpose. Each bit shows the status of the digital inputs but also allows commanding the inputs with MODBUS.

FAQ Subcategory:

This item was last updated on 03-05-2009
Document ID: 1052


The information provided in the AutomationDirect knowledge base is provided "as is" without warranty of any kind. AutomationDirect disclaims all warranties, either express or implied, including the warranties of merchantability and fitness for a particular purpose. In no event shall AutomationDirect or its suppliers be liable for any damages whatsoever including direct, indirect, incidental, consequential, loss of business profits or special damages, even if AutomationDirect or its suppliers have been advised of the possibility of such damages. Some states do not allow the exclusion of limitation of liability for consequential or incidental damages so the foregoing limitation may not apply.