AutomationDirect Logo General Drives Questions Frequently Asked Questions


« Return to the FAQ index

Question Are there any special considerations for motor grounding when using VFDs?
Answer Yes. The motor should have an appropriately size grounding conductor that is terminated at the dedicated VFD terminal. The motor ground conductor of a VFD has an induced current level that must be filtered through its source of origin. Thus a grounding connection needs to be made from the motor to the provided ground terminal on the VFD. An additional grounding terminal on the VFD connects to the common terminal board (comm. TB), which ultimately goes to the building grid ground. The above grounding procedures are necessary in order to reduce interference to the control circuitry as a result of the ground current induced from the drive.

FAQ Subcategory:

This item was last updated on 10-08-2007
Document ID: 1045


The information provided in the AutomationDirect knowledge base is provided "as is" without warranty of any kind. AutomationDirect disclaims all warranties, either express or implied, including the warranties of merchantability and fitness for a particular purpose. In no event shall AutomationDirect or its suppliers be liable for any damages whatsoever including direct, indirect, incidental, consequential, loss of business profits or special damages, even if AutomationDirect or its suppliers have been advised of the possibility of such damages. Some states do not allow the exclusion of limitation of liability for consequential or incidental damages so the foregoing limitation may not apply.