AutomationDirect Logo Relays and Timers Frequently Asked Questions


« Return to the FAQ index

Question What are the mounting options for the Fuji 1/16 DIN super timers?
Answer You can mount the timer either as a 'through the door' or as a back-panel timer. There are two different sockets for this and you must order an extra mounting clip for the 'through the panel' configuration. The TP411X and TP48X sockets will allow you to mount the appropriate timer on a 35mm DIN rail or directly to a backplane. The TP411SBA and TP48SB sockets will mount to the back of the timer when it's installed in an enclosure door, but you also need to order the PANEL-16 mounting clip to hold the timer flush against the enclosure.

FAQ Subcategory:

This item was last updated on 09-21-2007
Document ID: 1035


The information provided in the AutomationDirect knowledge base is provided "as is" without warranty of any kind. AutomationDirect disclaims all warranties, either express or implied, including the warranties of merchantability and fitness for a particular purpose. In no event shall AutomationDirect or its suppliers be liable for any damages whatsoever including direct, indirect, incidental, consequential, loss of business profits or special damages, even if AutomationDirect or its suppliers have been advised of the possibility of such damages. Some states do not allow the exclusion of limitation of liability for consequential or incidental damages so the foregoing limitation may not apply.