AutomationDirect Logo Pushbuttons Frequently Asked Questions


Press "Ctrl-F" to search for specific words in this FAQ.


Click here to view all Pushbuttons FAQs with answers on one page.

  1. What is the current draw of the Cutler-Hammer Lamps?
  2. What is hole size of your pushbuttons?
  3. Do you offer knockouts for pushbuttons?
  4. Do you offer a line of illuminated Emergency Stop buttons?
  5. What is the life expectancy of the E22HL3X8 bulb?
  6. Who makes your Centsable brand 22mm pushbuttons and switches?
  7. Are the Centsable 22mm and Cutler-Hammer E22 pushbutton products interchangeable?
  8. Why can I not replace the LED in the Cutler-Hammer Monoblock LED indicators?
  9. Can I use the Centsable LED replacements in both Cutler-Hammer and Centsable incandescent indicators?
  10. How many contact blocks can I use on the Centsable brand devices?
  11. What is the maximum wire size permissible with the Centsable contact block?
  12. These switches look very similar to devices I've seen in the past. Are the Centsable switches compatible with any other brands?
  13. Q: How much current does a 24VDC LED Light draw?
  14. Q: On the E22XBG1RR is the center position is it neutral?
  15. Q: Can you add a N/C contact to the E22PB3A?
  16. Why do red pushbuttons come with a standard NC contact instead of NO?
  17. Do you currently sell Maintained pushbuttons?
  18. How can I see if my contact is still working correctly?
  19. Im having a hard time removing the indicator lights from their sockets?
  20. What are the electrical ratings for the contacts on the HT8 30mm pushbuttons contact blocks?
  21. I need a contact closure for each position of my 3 position selector switch. How can I get that with the two Normally Open and two Normally Closed contacts you supply?
  22. What is the rotation of the ECX2300-5K ? How many degrees does it turn?


Troubleshooting Guides