AutomationDirect Logo GS Series Drives Frequently Asked Questions


Press "Ctrl-F" to search for specific words in this FAQ.

Would you prefer to narrow the list of GS Series Drives FAQs? Select a category from this list:

Related Drives FAQ Pages:


Click here to view all GS Series Drives FAQs with answers on one page.

  1. Will the DOP professional software work with the GS series of drives?
  2. How can I establish a minimum speed on the GS2?
  3. Can the GS1 drive perform dynamic braking?
  4. Can you control the GS drives with TND or Entivity studio?
  5. Can I use the MOP type terminal speed control with acceleration and deceleration times of less than 1 second? E.G. settings 14 and 15 for DI3-DI6 on GS2 and 14 and 15 for DI3 and DI4 on the GS1.
  6. Can I power the GS3 series drives from the D.C. Bus?
  7. My horsepower requirements fit either the GS2 or the Durapulse drive families,which is the best choice for me?
  8. Can I use these on electric vehicles?
  9. Is there a good way to do a master/follower with the VFDs?
  10. Does you have a cable/diagram for cable to connect my GS series drive to my DirectLogic or Click PLC?
  11. How can I set a higher maximum speed (RPM/frequency) than 60hz for the drive and motor ?
  12. Does the GS1 have Line Start Lockout feature like the GS3 ?


Troubleshooting Guides