AutomationDirect Logo IronHorse Motors Frequently Asked Questions


 

Use "Ctrl-F" to search for specific words in this FAQ.

Question: What style of motors do we carry?
Answer: Only NEMA frame motors.
For IronHorse, only TEFC (Totally Enclosed, Fan Cooled).
For Marathon, we have TEFC, TENV (Totally Enclosed, Non Ventilated), and TEBC(Totally Enclosed Blower Cooled) in different models.
Usually, higher horsepower motors will be the only ones to have a TEBC style.
MicroMax = TEFC 0.25 - 10 hp
BlackMax = TENV,TEBC 0.25 - 30 hp
BlueMax = TEFC,TEBC 40-100 hp
BlueChip = TEFC, TEBC 30-100 hp
FAQ ID: 1140

Question: What type of motors DON'T we carry?
Answer: DC motors
Explosion-proof
Metric
Washdown
Open Drip-proof
Single-phase above 1.5 hp
Type J frames
Wye-Delta
Dual or multi-speed motors
Other Marathon models,we can't order anything for them.
No Custom motors.
FAQ ID: 1142

Question: What is the shaft diameter in your CAD drawings?
Answer: Dimension "U" represents the shaft diameter.
FAQ ID: 1144

Question: What motors can be used with a drive (inverter)?
Answer: IronHorse can be used for straightforward applications, that don't require use below 360 rpm for pumpsor fans, or used below 900 rpm for winders or mixers. IronHorse always requires the use of a reactor (called a load reactor) between the motor and the drive.
FAQ ID: 1146