AutomationDirect Logo DL305 - DL350 CPU Frequently Asked Questions


 

Use "Ctrl-F" to search for specific words in this FAQ.

Question: I'm doing REAL number math and OUTing the value to a register with my D3-350. When I need that number it does not display correctly. What's wrong?
Answer: The REAL number PLC's use the IEEE 32 bit floating point format. You must use an OUTD to store the result of a REAL number math operation into V-memory.
FAQ ID: 97

Question: I'm upgrading my old DL305 systems to the new D3-350. How will my programs be handled?
Answer: The D3-330 and D3-340 use the old 305 instruction set. This is early to mid-80's technology. The new D3-350 uses the new 205/405 memory mapping and instruction set. Unfortunately the only way to convert is to rewrite the program. PLC Direct technical support does not offer this service but we can refer you to integrators who can rewrite your code if you do not wish to do it yourself.
FAQ ID: 99

Question: Does the D3-350 support ASCII/BASIC modules?
Answer: The D3-350 CPU does not support the ASCII/BASIC modules. The D3-330 or D3-340 do.
FAQ ID: 115

Question: Can you use an OP-CCBL to program a D3-350 CPU?
Answer: No...6;2-1 are jumpered together.
FAQ ID: 121

Question: Can I force I/O points in the D3-350?
Answer: I/O points in the D3-350 firmware version 1.15 or newer can be "forced" using bit override.
FAQ ID: 124

Question: What modules does the D3-350 not support?
Answer: D3-HSC, D3-232-DCU, D3-422-DCU, D3-HP, D3-HPP, F3-AB64, F3-AB64-R, F3-AB64-T, F3-AB128, F3-AB128-R, F3-AB128-T
FAQ ID: 352

Question: Will the D3-350 support the D3-04AD?
Answer: Yes, but only by using the multiplex method. You cannot use the pointer method and the PV direct access for the PID control because of the slow response of this module.
FAQ ID: 353

Question: Will the D3-350 support the D3-02DA?
Answer: Yes, but only by using the multiplex method. You cannot use the pointer method and the control output direct access for the PID control because this module has only 8 bit resolution.
FAQ ID: 354

Question: Where can I obtain the most current firmware for my CPU?
Answer: Go to the following links on our website to check for availability of firmware. Technical Support / Firmware Upgrades / Firmware Only.
FAQ ID: 395

Question: Will D3-HSC work with the D3-350?
Answer: No it will not.
FAQ ID: 663

Question: Does port 2 of the D3-350 have 5vdc?
Answer: No.
FAQ ID: 702