AutomationDirect Logo Encoders Frequently Asked Questions


 

Use "Ctrl-F" to search for specific words in this FAQ.

Question: What is the inside thread pitch of the TRD-N/NH Encoder?
Answer: 3 mil 16 x .5
FAQ ID: 487

Question: Do the hollow shaft encoders have the "Thru" hole or "Blind" hole?
Answer: They have the Blind hole.
FAQ ID: 619

Question: What is the basic definition of an encoder?
Answer: An encoder comes in two architectures. The first architecture is linear (which ADC does not currently sell.) The second architecture is rotary. Both types sense mechanical motion and translates the information (velocity, position, acceleration) into useful electrical data.
FAQ ID: 819

Question: What is the difference between an absolute and an incremental encoder?
Answer: There are a few subtle differences between absolute and incremental rotary encoders. Incremental encoders have output signals that repeat over the full range of motion. It is important to understand that each mechanical position is not uniquely defined. When the incremental encoder is turned on, the position of an incremental encoder is not known since the output signals are not unique to any singular position. Absolute encoders have a unique value (voltage, binary count, etc) for each mechanical position. When an absolute encoder is turned on, the position of an absolute encoder is known (this function resembles a resolver, although the principles of operation have no similarity.) The similarities of both absolute and incremental encoders are form factor and the issues of count and directional information. They can be obtained from both absolute and incremental encoders equally.
FAQ ID: 820

Question: What is a channel?
Answer: A channel is an electrical output signal from an encoder. Typical incremental encoders have either two or three channels. An example would be: A, A not, B, B not, and Z, Z not (also referred to I or I not.).
FAQ ID: 821

Question: What is quadrature and 4X (4 times) quadrature encoding?
Answer: Quadrature is a description of the 90 degrees out of phase between channel A and B. The rising edge to rising edge (referred as the Cycle) on channel A or B indicates that one set of bars (on the internal encoder disk) have passed by the optical sensor. The quadrature state of channels A and B create four unique logic states. Each group of four states is decoded as one directional count. These four unique logic states are decoded. 4x counting usually refers to a counter which may be configured to recognize each quadrature state as a separate count. So with this in mind 250 sets of bars would yield 1000 counts.
FAQ ID: 822

Question: What is the Index pulse (strobe, Z, and I.)?
Answer: It is the absolute reference added to an incremental encoder. It is also known as home position. It signifies a full rotation of the encoder disk
FAQ ID: 823

Question: How can I reduce the effect of noise when using encoders?
Answer: There are several ways to improve noise immunity. Be careful to separate motor and all power wires away from encoder wires. Always separate the channels from each other. All encoder wire should be shielded and carefully terminated. The pigtail that connects to the control unit using the encoder should be as short as possible. The leads will act as antennas for any stray RF in the vicinity. The addition of other noise suppression devices may be required in high noise environments.
FAQ ID: 824

Question: What are "Push Pull" and "Totem Pole" outputs? Why don't they have a differential output?
Answer: Looking at the A and A not channel, the optical sensor internal to the encoder is comparing the two. If A’s light amount is greater than A not, then A is high. When A is less than A not, then A is low. The same reasoning defines channel B. This process is called “Push Pull.” A “Totem Pole” output is the same as a “Push Pull” output. The big difference is the ability of the “Totem Pole” to handle sinking or sourcing less current than the “Push Pull.” It is confusing because the other factor is the amount of voltage usually used to define the difference between the two. “Totem Pole” usually uses 5vdc, where as the “Push Pull” follows the input voltage. Our encoders have a range of 5-30vdc, so you will see the output referred to as both. Our encoders that have “Totem Pole” outputs are technically categorized as open collector NPN style outputs. The only styles of differential encoder (5vdc) are our TRD – S/SHxxxx-VD models.
FAQ ID: 825

Question: Do I need to shut down my machine to change an encoder?
Answer: The best method is to power down the unit. If the supply voltage is accidentally shorted or grounded, it will damage the encoder.
FAQ ID: 826

Question: Q: What equipment do I need to troubleshoot an encoder?
Answer: A: An oscilloscope or specially designed encoder tester. A basic multimeter will do for basic diagnostics such as power supply and low speed pulse outputs. Any advanced pulse detection and diagnostics needs to be performed by a trained technician and an oscilloscope.
FAQ ID: 827

Question: Can you repair an encoder?
Answer: Yes, but we do not repair them. The issue is the cost of repair. A majority of the time, the repair costs more than the replacement.
FAQ ID: 828

Question: What is gray code?
Answer: Gray code is a form of binary. The difference is how it is incremented to the next number. Only one bit position can increment at a time. Gray code: 0, 1, 3, 2, 6, and 7 Binary: 0, 1, 2, 3, 4, and 5 We carry 8 bit /256 resolution thru 10 bit 1024.
FAQ ID: 829