Use "Ctrl-F" to search for specific words in this FAQ.
| Question: Can I change the Data Type of a Tag Name's assigned Address String (PLC Address)? |
| Answer: Yes, but only if the Tag is used on no more than one object. If it is currently used by more than one object, you must: a. assign the other objects to a new or different tag(s)—or delete those objects b. change the data type of the PLC Address under Setup > Tag Database c. re-assign the other objects to the original tag as necessary |
| FAQ ID: 527 |
| Question: Can the Tag Database be exported to DirectSOFT32 or other applications? |
| Answer: Yes, you must Have DSV4.0 or later and EZ Touch Edit V3.0 or later to do this. You can catually import Tags from DirectSoft too. |
| FAQ ID: 528 |
| Question: How do I convert a project from one panel size to another? |
| Answer: Converting a project created on a 6” panel to an 8” or 10” panel requires nothing more than opening the
project with the new size selected. Converting from 8” or 10” to 6” size is best done by the following procedure:
|
| FAQ ID: 529 |
| Question: Can I use the Power Up Screen selection (under the Project Attributes > General menu) and also use the Switch to Screen Number (under Project Attributes > PLC to Panel)? |
| Answer: Not exactly, because before the panel can actually display the Power Up Screen, it reads from the PLC and displays the Switch to Screen Number. |
| FAQ ID: 530 |
| Question: Can I place objects anywhere on the screen? |
| Answer: There are two types of objects in EZTouch Editor. One is Touch Objects (pushbutton, switches, numeric entry, etc.) and other is Display Objects (meter, bar graph, numeric display, line, circle, etc.) Touch Objects will always snap to touchcells, however, Display Objects may be placed anywhere on the screen. |
| FAQ ID: 531 |
| Question: What is a touchcell? |
| Answer: A touchcell is the physical area on the panel that defines user selection by touching. A Touch Object can contain more than one touchcell, but cannot contain less than one touchcell. On all EZTouch Panels, the size of a touchcell is 40x40 pixels. However, since the screen size differs, the physical size of 40 pixels does as well. On the 6” panels, 40 pixels = 0.57”. On the 8” panel 40 pixels = 0.52”. On the 10” panel 40 pixels = 0.41”. |
| FAQ ID: 532 |
| Question: Can I use the floating point data type with all objects? |
| Answer: Yes,however, you must have EZ Touch Edit V3.0 or later. |
| FAQ ID: 533 |
| Question: Why do I not see all the discrete tags in a pushbutton object? |
| Answer: You may have defined tags as discrete but if the PLC addresses assigned to these tags are read only addresses, then you will not see these tags. The reason is because a pushbutton writes discrete data to the PLC address and if a tag is mapped to a ReadOnly PLC address, the pushbutton is not allowed to write the data. |
| FAQ ID: 534 |
| Question: Can I use a label on a vertical radio button? |
| Answer: No, a label is not available for either vertical styled radio button or vertical styled tri-state button. |
| FAQ ID: 535 |
| Question: How does a radio button work? |
| Answer: A Radio button is assigned to a word (16 bit register) in the PLC. Each bit in the word (of this associated tag) corresponds to an individual button of the radio button object. Only one button can be ON at a time. So, turning one button ON automatically turns all other buttons OFF. |
| FAQ ID: 536 |
| Question: What is the initial state of objects when the project is written to the panel? |
| Answer: Once panel receives the project from the editor, it reads the PLC addresses associated with each tag and reflects the PLC’s status on the objects. So, the status of objects would reflect corresponding values in PLC addresses. |
| FAQ ID: 537 |
| Question: What will be the state of objects if they are mapped to internal tags? |
| Answer: Internal tags are initialized to OFF. |
| FAQ ID: 538 |
| Question: When I select a group of objects and try to move them, all the objects do not move. Why? |
| Answer: If you have selected a mix of touch and display objects and try to move this group, you will be able to move only display objects. Remember, touch objects are always snapped to a touchcell, whereas display objects are not necessarily snapped to touchcells. Try moving the touch objects first, then move the display objects. |
| FAQ ID: 539 |
| Question: When I have objects at the boundary of the screen, I am not able to move the objects freely (vertically up/down or Horizontally left/right near the boundary). What can I do to correct this? |
| Answer: You can use the PC’s keyboard arrow keys to move objects up or down along the boundary line. |
| FAQ ID: 540 |
| Question: What is the maximum number of screens that a project can have? |
| Answer: The maximum possible is 999. However, the panels memory may limit the achievable maximum to a lower number of screens, depending on the complexity of bitmaps and objects used in the project and their memory usage. |
| FAQ ID: 541 |
| Question: What is the maximum number of alarms that a project can have? |
| Answer: The maximum is 999, but there is no limit to how many times each alarm can be used in the panel. |
| FAQ ID: 542 |
| Question: What is the maximum number of messages I can have in the Message Database? |
| Answer: You can define a maximum of 999 messages in the Message Database. |
| FAQ ID: 543 |
| Question: Can I insert a 640x480 bitmap on a screen? |
| Answer: The maximum size of a bitmap that can ever be placed on a screen is 640x480 on a 8” or 10” panel. But, the compressed size of bitmap is also a limitation. The EZTouch panel uses an RLE (RunLength Encoding) algorithm to compress bitmaps for storage. If this compressed bitmap size exceeds 64K bytes, you cannot place the bitmap on the screen. |
| FAQ ID: 544 |
| Question: Is it possible to find out whether the compressed bitmap size is less than 64K before trying to insert the bitmap? |
| Answer: No, the only sure way to know is to try. An error message will alert you immediately if the 64K size is exceeded. Using fewer colors (like 256 vs. 24 bit) will help prevent this problem. |
| FAQ ID: 545 |
| Question: Is there a limit to the number of objects that can be placed on a single screen? |
| Answer: No, not exactly, but the maximum memory size of a screen is 128K bytes. |
| FAQ ID: 546 |
| Question: Will a line graph continue to trend if you are not on that screen? |
| Answer: Yes it will. The Line graph is the only part that updates even when the screen is not visible. |
| FAQ ID: 603 |
| Question: Will any touch panel display info from a 0-20mA device? |
| Answer: The only way is if the 0-20mA signal is connected to an analog card in a PLC that the touch panel supports. |
| FAQ ID: 604 |
| Question: Will the EZ-Touch panels be able to communicate to MUSHOSHITO PLCs ? |
| Answer: The only way is if the MUSHOSHITO PLC can communicate via Modbus protocol. |
| FAQ ID: 605 |
| Question: Does the EZ Touch panel have Boolean Expressions? |
| Answer: No, not at this time. |
| FAQ ID: 606 |
| Question: Does the EZ Touch panel have an Opto 22 driver? |
| Answer: Not at this time. |
| FAQ ID: 607 |
| Question: Will EZ Touch communicate to DSDATA? |
| Answer: No. Not at this time. |
| FAQ ID: 608 |
| Question: Does EZ Touch work with Think N Do 5.2 and earlier versions? |
| Answer: Yes. |
| FAQ ID: 639 |
| Question: With EZ Touch Editor can you put more than 1 button in the same location? |
| Answer: No. |
| FAQ ID: 667 |
| Question: When I open a project in EZ Touch Edit I cannot see the whole screen and I do not have any scroll bars. What could be wrong? |
| Answer: Check the Windows display properties and make sure your fonts are set to SMALL. If not, change it. |
| FAQ ID: 668 |
| Question: Can I scale my Numeric Display and Numeric Input Objects in the EZ Touch software? |
| Answer: Yes you can. |
| FAQ ID: 669 |
| Question: Will my EZ Touch software work with ThinknDo Studio versions 6.0 and 6.1 ? |
| Answer: Yes, but you must have EZ Touch version 1.01 or later. You can download free Maintenance Releases from our website. |
| FAQ ID: 670 |
| Question: Can the EZTouch access the ASCII table in the AB SLC5/03? |
| Answer: No. |
| FAQ ID: 725 |
| Question: What do I need to setup in EZ Touch Edit so I can change screens with my PLC? |
| Answer: Open an existing EZ Touch project or start a new one. Once you have an editing screen open choose SETUP>Project Attributes select the (PLC to Panel tab) notice the Item Switch to Screen Number (word). Assign a Variable memory address to this Tag (I.E. v2000 or N7:0 if using AB PLCs). Now all you have to do is move the number of the screen you wish to go to, to the assigned Variable memory location and the screen will automatically change. Note: If you are changing screens with the Switch to screen (WORD) in the EZ Touch software you will need to change the value in the register to a Value of a screen that does not exist ( I.E. 999) a few seconds after the screen changes to the desired screen. If you do not change the value in the register the panel will not change to a different screen if the value in the Switch to screen (WORD) has not changed. For example: If I tell the screen to go to screen 5 then change to another screen using pushbuttons on the screen, and something happens that would normally warrant the screen changing to screen 5 again. The screen will not change to screen 5 because the value 5 is already in the register and the screen will only change when it sees a change in the value in the (Switch to screen WORD register). |
| FAQ ID: 866 |
| Question: Where do I find the License Agreement for the EzTouch Software? |
Answer: It was saved on your PC when you installed the software.
|
| FAQ ID: 1253 |