AutomationDirect Logo Terminator I/O Frequently Asked Questions


 

Use "Ctrl-F" to search for specific words in this FAQ.

Question: What are the specifications for the T1K-DEVNETS module?
Answer: Those specifications can be found at this link.
FAQ ID: 488

Question: What are the specifications for the T1F-08DA-2 module?
Answer: The specifications can be found at this link.
FAQ ID: 489

Question: What are the specifications for the T1K-08TAS module?
Answer: The specifications can be found at this link.
FAQ ID: 490

Question: What are the specifications for the T1K-16TR module?
Answer: The specifications can be found at this link
FAQ ID: 491

Question: What are the specifications for the T1K-08ND3 module?
Answer: The specifications can be found at this link.
FAQ ID: 492

Question: What are the specifications for the T1K-16TD2 module?
Answer: The specifications can be found at this link.
FAQ ID: 493

Question: What are the specifications for the T1K-16TD1 module?
Answer: The specifications can be found at this link.
FAQ ID: 494

Question: What are the specifications for the T1K-16NA-1 module?
Answer: The specifications can be found at this link.
FAQ ID: 495

Question: What are the specifications for the T1K-08TD1 module?
Answer: The specifications can be found at this link.
FAQ ID: 496

Question: What are the specifications for the T1F-08DA-1 module?
Answer: The specifications can be found at this link.
FAQ ID: 497

Question: What are the specifications for the T1K-08TR module?
Answer: The specifications can be found at this link.
FAQ ID: 498

Question: What are the specifications for the T1K-08NA-1 module?
Answer: The specifications can be found at this link.
FAQ ID: 499

Question: What are the specifications for the T1F-08AD-2 module?
Answer: The specifications can be found at this link.
FAQ ID: 500

Question: What are the specifications for the T1F-08AD-1 module?
Answer: The specifications can be found at this link.
FAQ ID: 501

Question: What are the specifications for the T1K-08TRS module?
Answer: The specifications can be found at this link.
FAQ ID: 502

Question: What are the specifications for the T1H-EBC module?
Answer: The specifications can be found at this link.
FAQ ID: 503

Question: What are the specifications for the T1K-01AC Power Supply?
Answer: The specifications can be found at this link.
FAQ ID: 504

Question: What are the specifications for the T1K-01DC Power Supply?
Answer: The specifications can be found at this link.
FAQ ID: 505

Question: What are the specifications for the T1K-RSSS module?
Answer: The specifications can be found at this link.
FAQ ID: 506

Question: What are the specifications for the T1H-PBC module?
Answer: The specifications can be found at this link.
FAQ ID: 507

Question: What are the specifications for the T1K-MODBUS module?
Answer: The specifications can be found at this link.
FAQ ID: 508

Question: What are the specifications for the T1K-16ND3 module?
Answer: The specifications can be found at this link.
FAQ ID: 509

Question: What are the specifications for the T1K-08TA module?
Answer: The specifications can be found at this link.
FAQ ID: 510

Question: What are the specifications for the T1K-16TA module?
Answer: The specifications can be found at this link.
FAQ ID: 511

Question: What are the specifications for the T1F-16AD-1 module?
Answer: The specifications can be found at this link.
FAQ ID: 512

Question: What are the specifications for the T1F-16AD-2 module?
Answer: The specifications can be found at this link.
FAQ ID: 513

Question: What are the specifications for the T1F-16DA-1 module?
Answer: The specifications can be found at this link.
FAQ ID: 514

Question: What are the specifications for the T1F-16DA-2 module?
Answer: The specifications can be found at this link.
FAQ ID: 515

Question: Do you carry replacement fuses for the DC output modules?
Answer: Yes we do. Part T1K-FUSE ?1. They come in packs of 5 each.
FAQ ID: 516

Question: Do you carry replacement fuses for the AC & Relay output modules?
Answer: Yes, two different kinds. T1K-FUSE-2 is for AC/Relay output modules, and T1K-FUSE-3 is used for isolated AC/Relay modules. Both are sold in packs of 5 each.
FAQ ID: 517

Question: Can I use a Terminator EBC from a 405 ECOM?
Answer: This will not work. The ECOM will not work as a master. The Terminator EBC must be used with PC control.
FAQ ID: 602

Question: What version of Think & Do supports Terminator I/O?
Answer: 6.0
FAQ ID: 622

Question: How many T1K-IOCBL-1 expansion cables can you have per Terminator interface module?
Answer: The maximum number is 2.
FAQ ID: 763

Question: Is there any additional help on using the Terminator Analog cards using Modbus TCP etc..?
Answer: There is a series of PDFs on FACTS Engineering's website here;
FACTS Analog Info
FAQ ID: 1227

Question: What can I use to help debug/test Ethernet Terminator I/O?
Answer: FACTS Engineering has a Modbus TCP mastering program on their website Modbus TCP Master
FAQ ID: 1301

Question: What is the color code for American/Canadian thermocouples?
Answer: All American/Canadian Thermocouples follow the ANSI color standard for wire coloration. Jacket color may sometimes be the main wire color, but it is not a dependable means of thermocouple type.

Type J - White/Red
Type E - Purple/Red
Type K - Yellow/Red
Type T - Brown/Red
Type N - Orange/Red

Red is always Negative.
FAQ ID: 1310

Question: Do you have partnumbers for the Terminator removable connectors?
Answer:
    T1K-01AC - 6 pin terminal block
  • Manufacturer: Phoenix Contact Part #: MVSTBW 2.5/6-ST-5.08
  • Digikey.com part number 277-1066-ND
    T1K-RSSS â?? 4 pin terminal block
  • Manufacturer: Phoenix Contact Part #: MVSTBW 2.5/4-ST-5.08
  • Digikey.com part number 277-1064-ND
FAQ ID: 1321