AutomationDirect Logo Think & Do Frequently Asked Questions


 

Use "Ctrl-F" to search for specific words in this FAQ.

Question: I just upgraded to T&D 5.0. Now every time I go to run T&D I get "Data Logger Error" (No Runtime is available. Data Logging is not available at this time).
Answer: You need to replace the file (Tnddlog.exe) in the ThinknDo/Bin folder with this patch file. This fix is also indicated on a yellow or pink sheet of paper in the T&D box titled RELEASE 5 READ ME FIRST.
FAQ ID: 265

Question: What version of OP-Winedit software do I need in order for my OptiMate panel to communicate with Think & Do?
Answer: Use version 2.34 or higher. A free upgrade is available on our website here, but you must have a previous OP-Winedit package installed.
FAQ ID: 266

Question: Can Think & Do PC-based control software be used as a DeviceNet master?
Answer: Yes, it can.
FAQ ID: 267

Question: Does Windows 2000 support Think & Do software?
Answer: Yes, it does.
FAQ ID: 268

Question: Does the D2-Ctrint work with Think & Do?
Answer: No.
FAQ ID: 342

Question: Can I use T&D to multiple EBCs?
Answer: Yes, for PC Based T&D by using an Ethernet hub or switch you can have a maximum of 63 EBCs
FAQ ID: 409

Question: Is it possible to have Think N Do 5.2 and 6.1 installed on the same PC?
Answer: Yes, but 5.2 must be installed first. If 5.2 is already installed when installing 6.1 a Switch Utility will be installed allowing you to switch between the different packages.
FAQ ID: 641

Question: Im using a Think & Do PC and a WINPLC. Can I get DDE info directly from the WINPLC?
Answer: No. You must go through the Think & Do PC to get the data.
FAQ ID: 665

Question: What version of Think n Do supports Terminator I/O?
Answer: 6.0
FAQ ID: 726

Question: I have 2 or more network cards installed in a computer where both are using TCP/IP protocol. I can PING the WinPLC, but cannot connect using ESP.
Answer: When 2 or more network cards are installed in a computer, this is referred to as a "multi-homed" system.
The protocol manager needs to know which network card to send the TCP/IP packets over, and the WinPLC needs to know which one to respond to. This presents a requirement known as "IP Forwarding".
There are (2) requirements for resolving this issue.
1. You must enable IP Forwarding. This is handled differently for Windows NT and Windows 2000.
For Windows NT: Go to Control Panel->Networks->Protocols, and choose TCP/IP. Then click on the Properties button, and a dialog shall appear. Click on the tab labelled "Routing", and place a check mark next to "Enable IP Forwarding", then choose OK. Choose OK again to close the Network properties dialog, and reboot as instructed by the Windows NT.
For Windows 2000: WARNING: Using Registry Editor incorrectly can cause serious problems that may require you to reinstall your operating system. Microsoft cannot guarantee that problems resulting from the incorrect use of Registry Editor can be solved. Use Registry Editor at your own risk.
For information about how to edit the registry, view the "Changing Keys And Values" Help topic in Registry Editor (Regedit.exe) or the "Add and Delete Information in the Registry" and "Edit Registry Data" Help topics in Regedt32.exe. Note that you should back up the registry before you edit it. If you are running Windows NT, you should also update your Emergency Repair Disk (ERD).
Steps: a. Click on Start->Run, and type 'regedit' and press ENTER
b. Navigate to the key [HKEY_LOCAL_MACHINESYSTEMCurrentControlSetServicesTcpipParameters]
c. Find the value "IPEnableRouter", and double click on it You will now get an opportunity to change it's value. Change it to '1' (without the quotes) to enable IP Forwarding.
d. Reboot the machine to refresh the registry cache.
2. After enabling IP Forwarding, you must set the WinPLC's Default Gateway address to point to the Static IP Address of the Network Card that is connected to the WinPLC. This can be done through the standard "Reset using IPX", or if the WinPLC is available, through "Configure..." from ESP.
FAQ ID: 893

Question: I'm using Think&Do Live/Studio and I'm trying to connect to an H2/H4/T1H-EBC. But I keep getting errors.I have NetEdit and it can see the EBC with no problems. What could be wrong?
Answer: This problem is usually the result of having 2 NIC( Ethernet) cards installed in the same PC. If this is the case you need to access the network settings of the NICs specifically the Protocols that are assigned to each card. On the NIC that is used for your company you should disable/remove/uncheck the NWLink IPX/SPX protocol if installed. Then on the NIC card that is dedicated to the Think&Do system you should enable/install/check the NWlink IPX/SPX protocol and the TCP/IP protocol. You should also check to make sure that an address has been set on the EBC by toggling at least one dip switch to the ON position.
FAQ ID: 900

Question: I need to update my WinPLC to Live 5.4, but I can't find the update.bat program or the WinPLC runtime version 5.4 directory specified in the Updating a WinPLC system help procedure.
Answer: You need to run the Cetarget54.exe program in the CD's zoom directory.
This will install the update utility and the proper WinPLC runtime files on your PC.
You can then follow the Updating a WinPLC system help procedure.
FAQ ID: 938

Question: Does Think & Do or Studio work with Windows Vista?
Answer: Only version 8.0 and above support Windows Vista. Windows Vista does not support the IPX protocol nor does it support 16 bit program code. Versions of Think & Do and Studio before Version 8.0 used both IPX and contained 16bit program modules. Phoenix Contacts recommends disabling UAC
FAQ ID: 1064

Question: Is a demo version of Think & Do available?
Answer: Yes, TnD V 8 has a demo version here; Think & Do Demo
FAQ ID: 1071

Question: My ThinknDo Studio, TnD V8.x USB/Parallel key is physically damaged and no longer works. What can I do?
Answer: You can purchase the ESS (Extended Service Support) ESS-Basic or ESS-Premium support subscription. Damage to the key is covered and you will receive a replacement. You will have to provide the Serial number from the label on the damaged key when you purchase the ESS subscription.
FAQ ID: 1102

Question: Where can I find more support information for TnD or Studio?
Answer: You can find more help here;
Phoenix Contact Knowledgebase
and here
Phoenix Contact Think and Do 8.0
FAQ ID: 1103

Question: Where can I get the manual for TnD V8 ?
Answer: Think&Do V8 Manual pdf
FAQ ID: 1201

Question: TnD doesn't find my Setinel Key. Where can I get Sentinel Key drivers?
Answer: Sentinel Drivers
FAQ ID: 1218

Question: Can I upgrade from Studio to TnD V8.x ?
Answer:
    This can be accomplished using the Extended Service Support (ESS)package.
  • ESS-BASIC
      provides for Maintenance Updates.
  • ESS Premium
      provides for Major and Minor Version Updates as well as Maintenance Updates.

Purchasing ESS-Premium for your license of Think & Do Studio 7.1 provides for upgrading to the highest Minor Version Update 7.3 for example, and it provides for an update to Think & Do 8.0.
You can update to either as long as the ESS is in effect
FAQ ID: 1221

Question: What versions of Think & Do and MS Windows are compatable ?
Answer: Note! Windows 7 support is unknown at this time (11/24/2009)
The following applies to the 32 bit versions of Windows only.
TnD does not support the 64 bit versions of Windows
    TnD V8.x
  • Version 8 runs on Windows 2000, XP & Vista.
    Live!
  • Version 5.4 runs on Windows NT 4.0 (all service packs, Entivity recommends 6a) and Windows 2000 (all service packs BEFORE SP4). There is a workaround for 5.4 on XP on Phoenix Contact knowledgebase.
  • Version 5.5 and beyond runs on Windows NT 4.0 (all service packs, Entivity recommends 6a), Windows 2000 (all service packs), and Windows XP (all service packs).
    Studio
  • Version 6.0 through 6.51 runs on Windows NT 4.0 (service pack 6a) and Windows 2000 (all service packs).
  • Version 7.0 through 7.1 runs on Windows NT 4.0 (service pack 6a), Windows 2000 (all service packs), and Windows XP (all service packs).
  • Version 7.2 and beyond runs on Windows NT 4.0 (service pack 6a), Windows 2000 (service pack 2 and higher), and Windows XP (all service packs).

For more information consult the Phoenix Contact Knowledgebase
FAQ ID: 1274