Use "Ctrl-F" to search for specific words in this FAQ.
| Question: Is there a way to update the time and date on the touch screen to match the CPU clock of the PLC every time I power cycle the touch screen? I understand that the touch screen does not have a battery backed up clock. |
| Answer: Yes, this can easily be accomplished by placing an (External Clock part and an External Calendar part) - preferably ones with digital type displays. On the Global screen and under Access choose Closed and Selectable. Once this is done all the parts in the touch screen that pertain to date and time will now contain a time that matches the CPU clock (ie. warning displays that display a date and time). |
| FAQ ID: 259 |
| Question: When I try to communicate to my 250 CPU on port 2 RS422, I keep getting the error (#2965 CH3 Time Out error Check the cable and PLC station number). |
Answer: If you are using our D2-DSCBL-2 make sure that the wires are connected as shown on page A-4 of the Screen Creator manual and that blue/white is tied to green/white, and blue is tied to green.
If you are making your own RS422 cable make sure that it is connected as follows:
15 Pin Touch screen 7 ------------------ SG 10 ----------------- RD 9 ------------------ RD+ 6 ------------------ SD- 13 ----------------- SD+ Jumper 11-14 and 12-15 on the 15 pin port. |
| FAQ ID: 260 |
| Question: I cannot get my Allen-Bradley Micrologix PLC to communicate with my Touch Screen. I keep getting communication timeout errors. I have everything configured like the manual states on page A-6 of the Screen Creator manual. |
| Answer: The setup on page A-6 is correct except that Error Detection should be set to “CRC” to communicate properly with an AB Micrologix PLC. |
| FAQ ID: 261 |
| Question: What are the standard Modbus ranges in ScreenCreator? |
| Answer: Station Number : 00 to 99 Coil : 1 to 9999 Input : 10001 to 19999 Input Register : 30001 to 39999 Holding Register: 40001 to 49999 |
| FAQ ID: 262 |
| Question: How do I export / import a ScreenCreator project from one computer to another? |
Answer: Backing Up:
|
| FAQ ID: 263 |
| Question: I created several projects in Screen Creator v1.13 will they work if I upgrade to V1.17? |
| Answer: Yes. |
| FAQ ID: 264 |
| Question: My Screen Creator project acts like it is downloading to the panel but after it shows 100% I get an "unable to communicate with OIP". What is wrong? |
| Answer: Most likely you are using the wrong cable; make sure you are using the DP-PGMCBL. |
| FAQ ID: 408 |
| Question: Can Screen Creator program the EZ Touch panel? |
| Answer: No. It cannot. |
| FAQ ID: 613 |
| Question: Does Screen Creator work with Think N Do Studio Version 6.1? |
| Answer: No, Screen Creator does not work with 6.0 or 6.1. |
| FAQ ID: 640 |