AutomationDirect Logo ZIPLinks Frequently Asked Questions


 

Use "Ctrl-F" to search for specific words in this FAQ.

Question: Do you have any ZIPLink products that will work with the DL05 and DL105?
Answer: The D0-16TD1, D0-16TD2, and D0-16ND3 modules are compatible with the ZIPLink system.
FAQ ID: 228

Question: Are ZIPLinks only offered for select modules?
Answer: Yes - although modules appear to look the same, they are different in their AMP ratings. You can only use 2A max on the points and 4A max on the commons. The ZL-2CBL2-2P and ZL-3CBL3-2P pigtail cables may be used with I/O modules when there ia no pre-assembled cable available, provided the maximum amp ratings of the cables and ZIPLink modules are not exceeded.
FAQ ID: 229

Question: What ZIPLinks are supplied with the I/O terminal block already pre-wired?
Answer: ZL-2CBL1xx ZL-2CBL2xx ZL-3CBL2xx ZL-3CBL3xx ZL-4CBL2xx ZL-4CBL4xx ZL-CBL056 ZL-CBL056FR ZL-CBL056L Note: 64-point modules in the DL405 require two cables per module. Cables with "xx" in the part number are available in 0.5, 1.0, and 2.0 meter lengths. The "xx" in the part number is replaced by (blank) for the 0.5m cable, by "-1" for the 1.0m cable, and by "-2" for the 2.0m cable.
FAQ ID: 230

Question: What is the electrical life of the OMRON G2R-1 relay used on the ZL-CM08RL24 and the other 24vdc relay modules made by Ziplink?
Answer: The G2R-1 is rated: 1,000,000 operations at 0.5 A / 30 VDC inductive; 500,000 operations at 1 A / 30 VDC inductive and; 100,000 operations at 5 A / 30 VDC inductive. The rest of the specifications not found under the module specifications will be found at OMRON’s website. http://www.omron.co.jp/ecb/products/pdf/omron/english/en-g2r.pdf
FAQ ID: 912

Question: Where are the labels for my ZipLink module?
Answer: The stickers for the ZipLink products actually ship with the cables, since many modules are used with 3rd party devices, and the stickers would not apply. The pigtail cables do not include any stickers, since they are most often used with 3rd party products.
FAQ ID: 1219